cancel
Showing results for 
Search instead for 
Did you mean: 

MSC with sd card configuration

newbie
Associate II

I'm encountering an issue while attempting to configure my STM3240G-EVAL board to function as a “Mass Storage Device” with a microSD as Storage.

I used the MX configurator and followed tutorials but encountered the same issue every time. I can compile but if I connect the board via USB to my computer no device is detected.

 

Here's a breakdown of my configuration in MX:

SDIO and DMA:

  • SDIO is in “SD 4 bits Wide bus”-
  • DMA2 is active (SDIO_RX to DMA2 Stream 3 and SDIO_TX to DMA2 Stream 6)
  •  SDIO global interrupts are enable.
  • I tried different SDIOCLK clock divide factors (PCLK2 are 84MHz)

MSC:

  • USB_OTG_FS is “Device_Only”
  • Class for FS IP in USB_DEVICE is set to “Mass Storage Class”.

 

the other options are untouched.

 

Did I miss something or had somebody the same issue?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
newbie
Associate II

Hello @FBL 

I tried as USB host but it still not work.

One more time for me to understand.

I want to use my board as an USB-adapter for a microSD. if I connect the board to my computer the microSD will appear as drive on my computer so I can use it.

I was thinking in that case the board must be configured as device or did I missunderstood this?

View solution in original post

6 REPLIES 6
STTwo-32
ST Employee

Hello @newbie and welcome to the ST Community :smiling_face_with_smiling_eyes:.

First, you should use a data cable for communication not just a charging one.

Second, try using other COM ports of your PC.

Third, connect your board using the connector CN21 (ST-LINK/V2 connector) and not just any connector.

Best Regards.

STTwo-32 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @STTwo-32 

I use a data cable and the COM ports are working fine as well.

for the connection I use the CN8 USB OTG FS connector. 

 

To connect, you have to use the CN21 (ST-LINK/V2 connector) to connect your board using ST-Link.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I use the CN21 for flashing my board and also for the MSC?

I thought the USB OTG FS and the HS where for the MSC function.

 

But still if I connect the board after flashing the board via CN21 or USB OTG FS I dont get a connection between my sd card and my computer

FBL
ST Employee

Hello @newbie 

 

> if I connect the board via USB to my computer no device is detected.

You are using STM32 MCU as host ! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
newbie
Associate II

Hello @FBL 

I tried as USB host but it still not work.

One more time for me to understand.

I want to use my board as an USB-adapter for a microSD. if I connect the board to my computer the microSD will appear as drive on my computer so I can use it.

I was thinking in that case the board must be configured as device or did I missunderstood this?