User Activity

Recently I was confronted with a problem with TouchGFC in combination with ThreadX.I am developing a project with an STM32L4R7ZITx. The display is a 480x272 LTDC display. Everything was running smoothly until I changed the startup code for adding an ...
Hi all,I am in the process of bringing up a prototype board with a STM32L4R7ZIT6. I'm using CubeMX and use it for generating the startup code. I've configured a lot of peripherals.When I configure PG10 as an input, the CPU crashes. Exactly at the mom...
Hi all,I am in the process of bringing up a prototype board with a STM32L4R7ZIT6 up. I'm using one DAC channel via the opamp. This is working all right, until I designate the default output of the DAC to another function e.g. dig output. The DAC is c...
Kudos from