cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN transmitting wrong data and crashing peripheral

SvenBordihn
Associate

Hey, I am trying to send 20 messages over FDCAN using the G0B1RE Nucleo board. The problem is that only a few messages arrive (~12 most of the time), the messages have wrong data and sometimes it crashes the FDCAN-Module. When it crashes the HAL_FDCAN_RxFifo0Callback is not being called anymore, no more messages are being sent and no error code is generated yet all HAL FDCAN functions return HAL_OK.

 

I am sending the first message via HAL_FDCAN_AddMessageToTxFifoQ in my main loop and every following message in the HAL_FDCAN_TxBufferCompleteCallback

/*SENDING THE MESSAGES*/

FDCAN_TxHeaderTypeDef header;
header.Identifier = 0;
header.IdType = FDCAN_STANDARD_ID;
header.TxFrameType = FDCAN_DATA_FRAME;
header.ErrorStateIndicator = FDCAN_ESI_PASSIVE;
header.BitRateSwitch = FDCAN_BRS_OFF;
header.FDFormat = FDCAN_CLASSIC_CAN;
header.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
header.MessageMarker = 0;
header.DataLength = FDCAN_DLC_BYTES_8;

uint8_t buf[32] = {0};
memset(buf, 0x31, sizeof(buf));
memset(buf + 16, 0x55, 8);
for(uint8_t i = 0; i < 20; i++)
{
	header.Identifier = i;
	send_msg(phfdcan, header, buf + 16);
}

/* INIT */

hfdcan1.Instance = FDCAN1;
  hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV6;
  hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
  hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
  hfdcan1.Init.AutoRetransmission = DISABLE;
  hfdcan1.Init.TransmitPause = DISABLE;
  hfdcan1.Init.ProtocolException = DISABLE;
  hfdcan1.Init.NominalPrescaler = 1;
  hfdcan1.Init.NominalSyncJumpWidth = 16;
  hfdcan1.Init.NominalTimeSeg1 = 5;
  hfdcan1.Init.NominalTimeSeg2 = 2;
  hfdcan1.Init.DataPrescaler = 1;
  hfdcan1.Init.DataSyncJumpWidth = 16;
  hfdcan1.Init.DataTimeSeg1 = 1;
  hfdcan1.Init.DataTimeSeg2 = 1;
  hfdcan1.Init.StdFiltersNbr = 1;
  hfdcan1.Init.ExtFiltersNbr = 0;
  hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

I didnt want to include the whole send_msg implementation because it boils down to taking a message out of a buffer, checking HAL_FDCAN_GetTxFifoFreeLevel and transmitting it with HAL_FDCAN_AddMessageToTxFifoQ.

 

The problem was caused by the cheap USB-CAN Analyzer and not the st board. I verified this by using an Oscilloscope with a CAN decode feature

View solution in original post

2 REPLIES 2
mƎALLEm
ST Employee

Hello,

You need to debug the issue. Do you face Hardfaut exception?

what about send_msg() implementation?

send_msg(phfdcan, header, buf + 16);

 Since you're using  G0B1RE Nucleo board, are you using a CAN transceiver + another node connected to the bus? If not this is not a normal operation of CAN in Normal mode. Use Loopback mode instead.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I didnt want to include the whole send_msg implementation because it boils down to taking a message out of a buffer, checking HAL_FDCAN_GetTxFifoFreeLevel and transmitting it with HAL_FDCAN_AddMessageToTxFifoQ.

 

The problem was caused by the cheap USB-CAN Analyzer and not the st board. I verified this by using an Oscilloscope with a CAN decode feature