STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5 DCMI DMA is not working as expected.

Hello,    We have developed an image capturing application successfully based on STM32H7xxxx and OV7725 camera. We are now targeting to port the application to target STM32U5xxxx with the same camera. But it looks the DMA doesn't works as expected. T...

DCMI GPIO.jpg DCMI NVIC.jpg DCMI parameters.jpg GPDMA1 channels.jpg

Resolved! STM32G4 ADC offset correction in oversampling mode

Hello @Imen.D , A side question: RM0440 for G4 says oversampling mode does not support offset. Any change to this position as like the H7 change?  Solved: 'H7 ADC offset correction in oversampling mode - STMicroelectronics Community Thank you. SK

CSK by Associate
  • 366 Views
  • 3 replies
  • 1 kudos

Resolved! DFU issue after flashing STM32G0B0VET

Hey,  I am using the STM32G0B0VET (16MHz HSE) with a virtual com port over USB. The virtual com port is working fine but as a backup I would love to be able to let the user reflash the device. I was thinking of using the DFU for this since then the u...

Sander_V by Associate
  • 412 Views
  • 2 replies
  • 2 kudos

Resolved! SPI on STM32G071 not behaving as expected

Hi,i have  new design that i am migrating to the STM32G071 and having issues with the SPI1 port PB3,PB4,PB5. Changing CPOL and or CPHA during init code do not seem to have any impact, when powered down and restarted.I am seeing 9 clock pulses when se...

DS4_QuickPrint11.jpeg

Resolved! Power consumption of STM32H5 MCU for VIO Pins

Dear ST Team,I am using an STM32H5 series microcontroller in my design and I am trying to understand the overall power consumption contributed by different MCU interfaces.So far, I have identified the following:The typical maximum current on VDD, in ...

RajeshM by Associate II
  • 537 Views
  • 3 replies
  • 2 kudos