STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO F411RE timer in order to generate an interrupt

Learning on how to code 4x4 keypad with F411RE I came to need to learn timer in order to generate an interrupt (saying simply C function should be called lets say every 1 second) I created STM32 project CubeIDE+CubeMX  selected TIM3 (in Timers)  -> s...

Roman_E by Associate III
  • 716 Views
  • 12 replies
  • 2 kudos

Resolved! USB-PD attention callback never get's triggered?

Problem When i call * USBPD_PE_SVDM_RequestAttentionI get a OK message response but the callback never gets called.  * USBPD_VDM_SendAttention Curious to know if there's any good way to debug this?  Current debugging stepsI have a STM32G0-Disco board...

Current2.png Current capture.png Screenshot 2025-12-21 at 10.12.14 AM.png Screenshot 2025-12-21 at 10.01.39 AM.png

STM32N6 Power On sequence

Hello STM32N6 Tech support I am writing with reference to power on sequence. My power sequence is as follow1. First VDDA1V8_AON, VBAT and VDD is applied. My VDDIO4 & VDDIO5 is also connected with VDD.2. VDDCORE is supplied from an external SMPS step-...

STM32U5 internal RTC time greater than 24 hours

We are using the STM32U5 MCU and its internal RTC in our project.We are facing an issue where the RTC time sometimes goes beyond 24 hours — for example, we observed a timestamp showing 37 hours. The RTC is configured in 24-hour format, and we have in...

Resolved! STM32H5 ADC Measuring VREF+

Good morning,I would like to measure the supply voltage on an STM32H573RI. To do this, I measure VREFINT and then want to calculate the supply voltage.My approach (simplified):sConfig.Channel = ADC_CHANNEL_VREFINT; sConfig.Rank = ADC_REG...

afr_e2 by Associate II
  • 293 Views
  • 2 replies
  • 0 kudos

STM32H755 user button interrupt in both MCUs

Hello everyone, I would like to ask if it is possible (and if so, how) to make both m4 and m7 get an interrupt made by the user button in in the nucleo board, since the only Pin Context Assignment options on CubeMX is either m4 or m7. Do I have to do...

chrkaras by Associate III
  • 255 Views
  • 2 replies
  • 1 kudos

STM32H725 internal tamper detection

Hello,I am trying to figure out how to configure internal voltage monitoring use the internal tamper detection to clear the RTC when an undervoltage condition occurs. My understanding is that you have to enable the backup regulator and enable monitor...

Simon by Associate III
  • 475 Views
  • 2 replies
  • 0 kudos

ST-Link/V2-1 is not getting detected

  Hi,i am working on STM32cubeIDE for STM32G071RB nucleo-64 dev board with windows 11.i have a ST-LINK/V2-1 programming and debugging tool is integrated into the Nucleo as shown below image.To power the board, I connect the STM32 Nucleo-64 board to m...

Chhaleria_1-1768760222488.png Chhaleria_2-1768760645223.png Chhaleria_3-1768760937179.png