STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN2 Rx callback doesn't work STM32H753

Dear all,I'm struggeling to get FDCAN2 working on my board. I also use FDCAN1 - which is working pretty good.For FDCAN1 I selected the RxFifo0 and for FDCAN2 I selected RxFifo1.But for some reasons, I dont get the callback for HAL_FDCAN_RxFifo1Callba...

julred by Associate II
  • 5092 Views
  • 9 replies
  • 0 kudos

Resolved! Stm32G0b FDCAN automatic bus-off management

I decided to replace the STM32F105 with the STM32G0B in my project.I have problems setting up FDcan.The STM32F105 had an “automatic bus-off management” setting, but the STM32G0B does not! This feature is enabled by default, how can I disable it? So t...

Resolved! STM32H735G-DK and ADC usage

Hello, I have never used STM before and I am trying to choose a product, but I cannot buy and try each of them due to their prices. I am doing high-frequency work and I need a screen. STM32H735G-DK is a suitable board for me. However, there is a que...

Resolved! Have to choose between STM32H7B3 and STM32F7xx

Hello all, I have to develop an application with a 7 inch screen driver SSD1963,for the choice of cpu. I'm deciding between an STM32H7B3 and STM32F7xx, on the card I need RAM for screen storage,touchscreen management, communication with an FPGA in SP...

PSEBA.1 by Associate II
  • 2468 Views
  • 4 replies
  • 3 kudos

Resolved! MJPEG Video Decoding (stm32h747I)

Hi,I recently bought an STM32H747I-DISCO board and I'm trying to run the JPEG_MJPEG_VideoDecoding code example with an external display. The code works fine with the on-board display, but I'm struggling to get it working with an external display that...

AFato.3 by Associate II
  • 3370 Views
  • 2 replies
  • 2 kudos

Example Selector: FatFs_USBDisk -> FatFs_USBDisk_RTOS

I use NUCLEO-F767Z board and was working on a Application Framework that uses RTOS with different tasks, and logging to serial console and USBDisk. This is quite a while ago (STM32CubeIDE 1.6.1). I couldn't make USBDisk work with RTOS then. I switche...

FBerg.1 by Associate III
  • 5033 Views
  • 12 replies
  • 2 kudos