STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Query on STM32G473CEU3

Hi,We are using STM32G473CEU3 in our designWe have a situation that when MCU is powered off, 3.3V appears on one of the IO pins from an external circuit with 2mA of sourcing. Will this damage the MCU or is it ok?

PY.1 by Associate II
  • 1339 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L071 and ADC channel 5 and 6 rank

Hello, I have configure ADC to use channel 5 and 6 but I am not understanding what I am doing wrong to get readings from the two channels. Here is my code:void adcConvertionFinish(ADC_HandleTypeDef* handle); static ADC_HandleTypeDef g_adc; static co...

teobarbs by Associate
  • 1375 Views
  • 1 replies
  • 1 kudos

Resolved! Issue in STM32H563ZI SAI_DMA Configuration

Hi, I am using PDM mems microphone to configure the STM32H563ZI SAI_A with GPDMA. I have attached the image of configuration details. After configuration I generate the code, But GPDMA initialization details not showing in the code. //  main.c  file ...

Srmssenthil_3-1721826245915.png Srmssenthil_4-1721826318911.png

Problem with PSRAM peripherals of STM32H735

Hello! I use the OSPI2 interface of the STM32H735IGK6 to connect to the ISS66WVO32M8DBLL and use indirect mode for memory reading and writing.1、The first step is to use cubemx to configure OSPI interface parameters as shown in the following figure:  ...

Lin_Yishan_0-1722994715086.png Lin_Yishan_1-1722994714722.png Lin_Yishan_2-1722994715331.png Lin_Yishan_3-1722994715328.png

Resolved! Up-to-date version of USB-PD "demo" wiki seems broken

Ok, so I tried to follow https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink for an example on how to use STM32G0B1 family as a simple USBC Power delivery sink. The Article seems to have received an update o...

Franz.1 by Associate III
  • 3034 Views
  • 5 replies
  • 0 kudos

STM32F103 Circuit Issue

Hi Everyone,I am working with an STM32F103C8T6 chip on a project.  For some reason I cannot flash the chip. It connects everytime I try though. I am using the SWD to flash. Is there anything you notice that is incorrect on or may be affecting the cir...

1000007748.jpg
Fmukete by Associate
  • 5482 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.