STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F446RET6R TWO CAN PERIPHERALS

Hello!! I'm trying to use both CAN peripherals in an STM32F446RET6R on a custom PCB, but something is not going well enough. I've done the basic configuration using the STMCubeIDE platform (I'll add the code later, but first I want to know if someone...

Davaol19 by Associate III
  • 12607 Views
  • 30 replies
  • 2 kudos

Startup time of NUCLEO G431RB varies greatly

After troubleshooting this issue , i found, that i have a greatly varying startup time.I have this minimal code:int main(void) { /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); GPIO_InitTypeDef my_GPIO_InitStruct = {0}; // TEST PIN ...

Tobe by Senior III
  • 1577 Views
  • 2 replies
  • 0 kudos

Resolved! Unknown chip id! 0x421

Hello, so I am completely new to working with STM boards in general. I just got a brand new stm32f446re board, and I tried to upload some code to it through Linux. And I do mean brand new, I haven't uploaded or downloaded any code to it before this a...

Odega by Associate II
  • 11738 Views
  • 25 replies
  • 1 kudos

Resolved! netxduo mqtt application

Hallo,I have to question, all about netxduo.1. how to set the pool size of netxduo at the least value possible2. I need to use the mqtt client packet.  Is it necessary also to enable the arp protocol, icmp protocol, the TCP protocol, the udp protocol...

IVent.1 by Senior
  • 1309 Views
  • 1 replies
  • 0 kudos

two timer signals on one pin

Hi,Here is my problem, I need to output two different frequencies on one pin and I can't reconfigure the timer to new arr/psc values for a different frequency because these timers also output the frequency on other pins where the frequency/timer conf...

RLD by Associate II
  • 3126 Views
  • 7 replies
  • 0 kudos

Recommended resistor and power ratings for STM32F105 ADC

We are using STM32F105 ADC function in some of our products for temperature sensing, etc. We found that sometimes it has accuracy issue after operating for a while. We suspect that it's the power, resistor, or capacitor we used are not of good enough...

WXWorkCapture_17264644812107.png
ax369 by Associate II
  • 1263 Views
  • 1 replies
  • 0 kudos

Resolved! modbus tcp-ip (server/client) Over ethernet

Hi ,I need example modbus tcp-ip (server/client) Over ethernet,As i have to create Modbus tcp ip communication from scratch (develop Modbus stack for better debugging )Any one suggest where i have to start with some dev board along with some existing...

Ss.61 by Associate III
  • 4704 Views
  • 8 replies
  • 3 kudos

Resolved! Object detection

Hi all,I am trying to implement object detection algorithm on STM32F429 - DISC1 model with MATLAB Simulink. I didn't use earlier. So, please guide to me "How to implement software into that."