STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART error in STM32F4

Good evening community members,today I have been trying to activate USART module of my STM32F446 board. However even after trying everything, I could not sense Tx signal on PA2 pin of the board. This is the low level code I used. I had been trying to...

Issue when using SPI using DMA

Hello,  I wanted to have SPI with DMA RX, below issues I face: 1. When SPI RX DMA function used with no TX DMA configured in MX (but blocking SPI TX used), It remains in RX busy state 2. When SPI RX DMA function used with blocking TX function, SPI wo...

GauravK by Senior
  • 1021 Views
  • 0 replies
  • 0 kudos

Resolved! Perform fft on stm32f411

I am trying to make a music visualizer with led matrix and stm32f411 usb audio functionpreviously , i tried to use stm32f103 blue pill but the usb audio stuck and i can't find the reasonso i purchased the black pill to do it but now the problem is th...

Enabling ADC Offset

Hi,I'm trying to apply an Offset on the ADC, I'm using a H743. I'm pretty sure I have the ADC working correctly, because measuring temperatures (MCU internal and one external) as well as measuring some voltages on my board result in plausible values....

Hazardy by Associate
  • 1096 Views
  • 0 replies
  • 0 kudos

Resolved! clock configuration issues when I use CAN

good morning. I want to implement a can loopback on my STM32H755, but when I enable FCAN1, then my clock can't resolve it issues and shows this for FDCAN in the picture below. how could I resolve this problem?  

Jad_0-1726221753821.png
Jad by Senior
  • 4227 Views
  • 9 replies
  • 0 kudos