STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MIPI DSI Display required for STM32H747XIH6

Hello all,Im looking for LCD Display that I wanted to interface using ST32H747XIH6 Microcontroller, with its MIPI DSI 2 lanes interface. I see it can only support upto 800x480 in the datasheet, or am i wrong?, can the MCU drive larger resolutions lik...

Arrvinddd_0-1715259206121.png
Arrvinddd by Associate II
  • 8090 Views
  • 7 replies
  • 0 kudos

Trying to understand workspaces and projects

Posted on March 04, 2017 at 19:17I've used various microprocessor dev systems for several decades, but am new to Eclipse and STM32.I bought a STM32L476G-EVAL board, installed the SW4STM32 toolchain, downloaded the STM32L4 firmware package and placed...

SPI slave master DMA 4Mhz not working

Hi,I am using a STM32H5 as SPI slave DMA (the main clock is at 250Mhz and SPI clock is at 160Mhz)... I am trying to receive data (2072 Bytes) from a master with a clock of 4Mhz and I am having some OVVERUN is this normal. When the master clock is at ...

aabba.1 by Associate III
  • 2942 Views
  • 6 replies
  • 5 kudos

Resolved! Variable rolling to 255

I have STM32G070RBT6, a timer is set to give interrupt every 1 second, in interrupt i am incrementing a variable timer_var1 then in main file while loop i am dividing this by 10 and assigning this value to another variable TIMER_NOW. Now when timer_v...

snip1.png snip2.png
psain.1 by Associate III
  • 8725 Views
  • 11 replies
  • 3 kudos

Resolved! STM32F1 canbus problem zephyr

Hello everybody,I try to get canbus communication on the blue pill+ under zephyr to work. I use the canopennode sample. I got the following overlay: / { model = "STM32 Minimum Development Board (Blue)"; compatible = "stm32_min_dev_blu...

eiten by Associate II
  • 3260 Views
  • 5 replies
  • 1 kudos

Resolved! STM32L152RET6 bootloader via huart3

Is it possible to use UART3 as the bootloader interface on this chip?I’m able to communicate with UART3 (so the hardware connection seems fine), but I’m unsure about the baud rate—does the bootloader autodetect it, or is it fixed? The bootloader work...

mt1 by Associate II
  • 1860 Views
  • 3 replies
  • 0 kudos

STM32F4 - FFT for 32768 input buffer

Posted on October 16, 2014 at 14:31Hi everybody!I'm going to use STM32f429 with external SDRAM (IS42S16400J 64MBit) in my project. I'm trying to make FFT for 32768 input buffer, my function calculate it in about 250ms.Functions in CMSIS LIB do it mu...

Resolved! RM0360 and stm32f030xc.h TIM7 IRQ discrepancy

I am designing a board based around the STM32F030RC, and noticed an apparent discrepancy on IRQ18 between materials.STM32CubeMX allows both TIM6 and TIM7 to generate interrupts, and the stm32f030xc.h file it generates defines TIM6 as IRQ17 and TIM7 a...

STMCubeMXpng.png Table 31. Vector Table.png
Haruki by Associate
  • 1680 Views
  • 2 replies
  • 1 kudos