STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! GPIO connections of OCTOSPI on external flash and ram

My MCU is the STM32H723. To save GPIO pins, I would like to use the following architecture:- Connect external HyperRAM and Flash to one OCTOSPI bus. - Use multiplexed mode to access OCTOSPIM_P1 and OCTOSPIM_P2.- Map external RAM and Flash to differen...

STM32G4 chaos in internal ref

Hi, i start design on G4 and am confused with internal ref in MX.1. Internal REF for ADC isnt real internal, but Vref2.Internal ref for comparators is 1/2 1/4 3/4 ... , but from what ?3. ADC stop working without VREF+ pin voltage, but comparator work...

MM..1 by Chief III
  • 1603 Views
  • 0 replies
  • 1 kudos

Need help with specific I2C DMA setup on STM32U5

Hello,I am trying to implement the following: a timer (tim3) is set to PWM generation, outputting a pulse periodically. Its TRGO triggers the DMA channel to request I2C to initiate a read transaction, read 8 bytes and generate an event interrupt (TC ...

ruddy17 by Associate II
  • 5865 Views
  • 5 replies
  • 1 kudos

Implementing MQTT in STM32F407G

Hi Team,I am currently working on a project involving the STM32F407G microcontroller, where I have configured MQTT to connect to a server. However, I am encountering persistent issues and have been unable to establish a successful connection.The spec...

ggowd.1 by Associate III
  • 22105 Views
  • 12 replies
  • 1 kudos

Resolved! UART Transmitting issue or any other issue

Hi Everyone, I am using STM32F407DISCO board and made a simple program which transmit some values. The program is as follows   #include "stm32f4xx_hal.h" #include "main.h" UART_HandleTypeDef USART2Config; void GPIO_Init(void); void UART2_Init(void...

AHayee_0-1726491245079.png AHayee_1-1726491391625.png
AHayee by Associate II
  • 3307 Views
  • 8 replies
  • 1 kudos

Resolved! task doesn't start when run in ram

hello:    I use NUCLEO-H7A3ZI-Q to test a bootloader feature:the bootloader runs in 0x08000000 at flash, when it starts, it copies the application stored in 0x08005000 to 0x24000000 in RAM, then jump to 0x24000000, I turn on a led in main function to...

lbapplem by Associate II
  • 1797 Views
  • 3 replies
  • 2 kudos

Where can I download Unico-GUI

Hello everyone,I am designing an application with a machine learning core device (LSM6DSOX). I attended the webinar on machine learning core last week and following the tutorial from this webinar I need to use Unico-GUI software tool.I tried to dowlo...

Jmong.1 by Associate II
  • 2524 Views
  • 3 replies
  • 0 kudos

USB between two MCUs & host PC

I am looking to design a split keyboard that requires USB communication between two keyboard halves and  a host computer. The left half will have a USB-C connection to a host computer and appear as a USB HID with regular keyboard functionality. This ...

Hayden by Associate
  • 1622 Views
  • 2 replies
  • 0 kudos

Resolved! How to connect 8 SRAMs to STM32H7

Hello everyone.I want to connect 8 SRAMs (2MB) to STM32H755XIH3 and use them as 16MB work memory.When connecting 8 memories (SRAMs) using FMC (devices more than the number of FMC_NE*), how should I connect and control them? If there are any similar c...

kazutobi by Associate II
  • 5722 Views
  • 13 replies
  • 5 kudos