STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H5 getUID with enabled ICACHE

Hi. Is there any consideration that I need to take care of when I use HAL_GetUIDw0~2 while ICACHE is enabled?even the simplest project with STM32H573IIK3Q that the ICACHE is enabled will get a hardfault when trying to get UID bytes.This is the whole ...

Absolute minimum One Pulse response time STM32H757

Is the minimum response time of a OPM trigger defined anywhere?  I'm measuring a delay of 50-100ns.  I was hoping it would be at maximum a couple clock cycles, but I may be naive. Running on CM4 at 200MHz of the STM32H757i-eval, using Timer8, Trigger...

JJordan_0-1728416552772.png
JJordan by Associate II
  • 5011 Views
  • 10 replies
  • 7 kudos

Using STlink /V2 to program my NUCLEO-F103RB

I am trying to talk to my NUCLEO-F103RB board via my st-link/V2 B202016 but so far I have not been able to. Below is an image of my connectionBelow is an image of my jtag connect I have connected the pins in following order JTAG_Pin 19 -> (Nucleo Boa...

BadEngineer_0-1728579809590.png BadEngineer_1-1728579880544.png BadEngineer_2-1728580630787.png

ADC multichannel wacthdog interrupt

Hi all.I'm working on a project with STM32H7 and I've got a question:I'm doing some experiments with ADC multichannel and wacthdog enabled to launch an interrupt of One of the Channel measured level passes the alert level (High threshold).Everything ...

zioMorgan by Associate II
  • 2974 Views
  • 7 replies
  • 1 kudos

Resolved! Trying to access STM32L072CZ AHB2 addresses from SWD

Hi,New to STM32 I'm discovering the STM32L072CZ, I'm trying to access the AHB2 bus by SWD interface in order to r/w on addresses (say 0x4800 0000 on peripheral GPIOA). When performing a coresight read on 0x48000000 I got 0xBC11477.After checking Ultr...

NKA by Associate II
  • 1353 Views
  • 2 replies
  • 1 kudos

Resolved! Error in RM0490 Rev. 4 Section 6.2.6

Status bits in the RCC internal clock source calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.Should be the following:Status bits in the RCC clock control register (RCC_CR) in...

MorganG by Associate
  • 1473 Views
  • 2 replies
  • 1 kudos

DP83848 Tx not working

Hi all,we have a custom board with STM32H753 MCU and a DP83848 PHY. When configuring the PHY in loopback mode I can send and receive messages as expected. But when not in loopback mode we can receive data but the Tx path is not working.As the loopbac...

ingdb_2-1728335342319.png
ingdb by Associate II
  • 3104 Views
  • 6 replies
  • 0 kudos