HI, STM Experts, Using STM32CubeIDE, I configured a project with default settings for the STM32H563ZIT6 (8 MHz external clock), running at 250 MHz. Additionally, I've enabled SPI1 for full duplex communication (transmitting and receivi...
Hi, I would like to check whether it is possible to perform internal SPI full duplex loop back tests on the STM32H563ZIT6 board, but I don't know how to do it.any one please help me.
Hi,I'm trying to interface audio output to the STM32H563ZIT6 microcontroller. I want to use GPDMA1 with the DAC, but I don't know how to configured GPDMA1 on STM32 CUBE IDE. Can anyone help me, please?
HI,i am trying to interface the HX711 Load Cell to STM32G0B1RCT6 Microcontroller.i using internal clock source(HCLK = 16MHz) and its reading good.Load Cell Value: 8220309Load Cell Value: 8221048Load Cell Value: 8221228Load Cell Value: 8221368Load Ce...
Hi, I am using the STM32H563ZIT6 microcontroller and trying to interface it with an internal DAC to a speaker through an external MCP601 op-amp. I am generating a sine wave on that DAC pin, but it is producing some noise in the speaker. I am unsure h...
sorry for my post its working good but i have an doubti am testing loop back test on spi1 on stm32h563zit6 microcontrollerhardware connection:spi1:mosi---------->miso uint8_t tx_buffer[] = { 'H', 'e', 'l', 'l', 'o', '\r', '\n' };uint8_t rx_buffer[20]...
now i am connecting that to transmit data from SPI1 to SPI2 on the STM32H563ZIT6 spi2--->full duplex master spi3---->full duplex slave spi2_clk to spi3_clk spi2_mosi to spi3_miso spi2_miso to spi3_mosiuint8_t txData = 0x55; // Example...
For SPI checking purposes only, whether to transmit data from SPI1 to SPI2 on the STM32H563ZIT6 microcontroller or to perform a single SPI transmit and receive operationtell me single spi transmit and receive hardware setup