Skip to main content
HDesa.1
Associate III
June 19, 2024
Solved

STM32H7 dual core: FreeRTOS & Timer selection for each core

  • June 19, 2024
  • 3 replies
  • 1869 views

Hello,

I am using STM32H7 dual core series. Currently I am planning to enable FreeRTOS in M4 core and let M7 core run in regular fashion.

As FreeRTOS uses SysTick, I have given M4 core on of the controller timer. Is there any need to also give M7 core a different timer? As M7 core is not running FreeRTOS, can it continue running on SysTick timer.

-Regards

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

Each core has its own system tick timer. Each core has its own program to run and using systick or not on CM7 doesn't change anything in your scenario.

https://developer.arm.com/Processors/Cortex-M4

https://developer.arm.com/Processors/Cortex-M7

 

3 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
June 19, 2024

Hello,

Each core has its own system tick timer. Each core has its own program to run and using systick or not on CM7 doesn't change anything in your scenario.

https://developer.arm.com/Processors/Cortex-M4

https://developer.arm.com/Processors/Cortex-M7

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
HDesa.1
HDesa.1Author
Associate III
June 22, 2024

Thank you for the clarification.

This means I can definitely run one core in a loop & other core using FreeRTOS, right?

Also if I need to communicate between the cores then I can still use Openamp middleware.

-Regards

-RegardsHrishikesh
mƎALLEm
ST Technical Moderator
June 22, 2024
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.