User Activity

Hi,I am using the PWM1 mode of the STM32G031 TIM1 and I noticed that the rising and falling edge time of its PWM output is about 20 ns. I have used the PWM fast mode but this time is not getting shorter. I would like to know if this time is normal? B...
Hi,I would like to know the meaning of each data in the L4CX calibration data(VL53LX_CalibrationData_t in API), because there is a lot of data for this IC, and I would like to confirm the status of the calibration from the data.Thank you.
HI,The driver file I downloaded from the official website is version 1.2.8.(stsw-img029)But when I downloaded the Demo(X-CUBE-TOF1), I found that it uses version 1.2.10.Should I use the latest one? Thanks
The VL53L3CX API‘s example code use 12KB of RAM, which makes it impossible for me to try to use the program with a smaller RAM MPU.The example for L1X,L0 are not the same, they only use about 2KB of RAM.I would like to know if it is necessary to use ...