User Activity

Hello,I would like to run a ML model which I had created using tflite on the STM32H7 series. I have installed x-cube-ai 8.1. Are there any tutorials or manuals where I can understand the functions to be used.There are a few videos but those are the o...
Hello,I am running a NAND flash with STM32H7 microcontroller using FMC interface. I have referred to Using the high-density STM32F30xxD/E FMC peripheral to drive external memories datasheet for the programming purpose.While communicating with the dev...
Hello, I am using STM32H7 dual core series. Currently I am planning to enable FreeRTOS in M4 core and let M7 core run in regular fashion. As FreeRTOS uses SysTick, I have given M4 core on of the controller timer. Is there any need to also give M7 cor...
Hello,Can anyone help me with interfacing NAND flash with STM32H7 microcontroller? I am unable to find any reference guide or application note related to the same.-Regards
Hello,Could you please help me with handling a same channel I2C protocol between 2 core.I have two devices connected on the same I2C channel(I2C1). I want to run one device on M7 core and another on M4 core. How to handle the communication between th...
Kudos from