STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NVIC - Defining software interrupt

Posted on August 08, 2013 at 08:37 Hi , I want to add a new interrupt to the system , i know that the NVIC can support up to 256 interrupts , currently in my evaluation boad ( stm32f4g-eval) there are only 81 used . So i added a new on...

Why is DMA reducing my pulse width?

Posted on August 01, 2013 at 03:43Howdy,     So I enabled DMA1, on STM32F103, copying two 32-bit words (set and clear PF.15) from flash to GPIOF->BSRR at 25kHz.  I then run this code with all interrupts disabled while(1) {     GPIOF->BSRR = 1 << 14;...

bikejog by Associate II
  • 8105 Views
  • 20 replies
  • 0 kudos

STM32F4 Free running 32-bit timer/counter

Posted on August 07, 2013 at 20:14Can someone please point me in the right direction to use TIM2 or TIM5 as just a free running 32-bit counter, ticking at 1us, that I can read anywhere in my pgm.  No I/O or interrupts desired. None of the examples i...

USART NOT receiving nothing

Posted on August 07, 2013 at 07:12Im using usart2 and i know its sending data but will not receive im using :rx_data = USART_ReceiveData(USART2);to save the data then using a while(rx_data > 0 ) { do stuff}any suggestions about why its not receiving...

timothy by Associate II
  • 3377 Views
  • 6 replies
  • 0 kudos

programming problem after Remapping PB3 & PB4

Posted on August 07, 2013 at 10:35Hello, I equipped the Header of the STM32F100RB-VL Dicovery Board with some LEDs. But then I recognised that PB3 and PB4 are not working, because they have to be remapped. Since this remapping I`m not able to flash ...

Is there STM32F051x8 in stop mode has a 1ms timer

Posted on August 05, 2013 at 09:43Hi,I am using the STM32F051x8,I want a timer which could interrupt every 1ms in the stop mode?But I have found the TIM can't work in the stop mode,and the RTC just happen interrupt every second. How can I do?Thanks?...

USB OTG and AHB clock

Posted on August 07, 2013 at 07:29I would like to know that is there any minimum value of AHB if USB OTG is needed?The MCU that I'm using is STM32F105/7 which is in connectivity line series.When I set my SYSCLK to 48MHz or 72MHz and AHB prescaler is...

jlim by Associate
  • 682 Views
  • 0 replies
  • 0 kudos

[STM32L] ADC channels and sampling rate

Posted on August 07, 2013 at 03:03Hi all.In the datasheet and reference manual,  it mentioned STM32L1xxRx has 1 ADC module with 20 channels.  I know that 12-bit resolution, the maximal sampling rate could be up to 1Msps.My question is, if I use 5 an...

can't write to peripheral register

Posted on August 06, 2013 at 21:14I have begun programming the stm32f4.  I made a really simple program first.  It added one to r0 and stored the result in r0.  Then I used STM32 ST-LINK utility to confirm that r0 is increasing.  It was.  I though I...

drobison by Associate II
  • 2864 Views
  • 4 replies
  • 0 kudos