cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 TIM2_CH1

npham
Associate II
Posted on September 20, 2012 at 20:07

Hi,

Looking at the data sheet of the STM32F407X, I can't find what pin number the TIM2_CH1 maps to. Please help. Thanks

Nhan Pham
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on September 20, 2012 at 20:18

PA0, PA5 or PA15

Described in at least two places the 40X manual DM00037051

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
npham
Associate II
Posted on September 20, 2012 at 20:58

The pins you pointed out are for TIM2_CH1_ETR. I thought they have different function than the TIM2_CH1 pin. Please clarify. Thanks

Nhan Pham

Posted on September 20, 2012 at 21:40

TIM2_CH1_ETR is TIM2_CH1 and TIM2_ETR

TIM2_ETR is an input, so you'd use it while not using TIM2_CH1 as an output.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..