cancel
Showing results for 
Search instead for 
Did you mean: 

EXTI pending bit not cleared by edge detector setting change as promised

waclawek.jan
Super User
Posted on September 21, 2012 at 18:08

The ST32F4xx user manual, RM0090, on page 205, for the EXTI_PR (pending register) bits says:

> This bit is cleared by writing a 1 to the bit

> or by changing the sensitivity of the edge detector.

The latter one does not appear to be true - changing the corresponding bit in either the EXTI_RTSR or EXTI_FTSR register does not have influence on the state of EXTI_PR register.

A simple test routine below - should end with EXTI_PR in 0, but on the eval board I have at hand it ends with EXTI_PR == 1.

While strictly speaking this is not a bug and it's trivial to work around (simply using the first method); it is at least a documentation error.

Could anybody please confirm or reject?

Thanks,

Jan Waclawek

 EXTI->RTSR = 0;   // both edge detector setting registers set to 0

  EXTI->FTSR = 0;   // (they are 0 by default, but just to be sure)

  EXTI->IMR   = 1;  // unmask interrupt for 0th bit

  EXTI->SWIER = 1;  // this forces the _PR register to 1

  __asm(''nop'');     // here check that _PR is indeed 1

  EXTI->SWIER = 0;  // shouldn't really be needed

  // changing the edge detector should clear the pending _PR bit

  // we can try changing either rising or falling

  EXTI->RTSR = 1;

//  EXTI->FTSR = 1;

  __asm(''nop'');     // okay so here _PR should be 0 again

#exti
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0