STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO_Remap_SWJ_Disable Issue

Posted on August 08, 2013 at 23:20 Hey guy's ! [I'd like to apologize for my bad englisch] I think I've made two mistakes in a row... First, I designed a STM32 Board with the usage of the Pin PA.15 - which is remapped after ...

benedikt by Associate II
  • 2113 Views
  • 2 replies
  • 0 kudos

CMSIS DSP PID Algorithm and 1.15 format

Posted on August 10, 2013 at 04:51Hello, I am having a problem with CMSIS DSP. the state variables are represented in 1.15 format.I want to control the speed of a motor using PID algorithm.The minimum value of the PWM duty Cycle is 500 and it Maximu...

STM32W108xx IRQC configuration

Posted on August 06, 2013 at 19:20 Hello all, I'm working on STM32W108xx & interfacing a sensor whose interrupt pin connected to the PB7, IRQC pin. How to configure this pin for the following handler ? void EXTIC_IRQHandler( void ) ...

harinath by Associate III
  • 1448 Views
  • 3 replies
  • 0 kudos

How to unlock SWD on STM32F0?

Posted on August 09, 2013 at 10:15Hi, I accidentally configured USART2 to pins PA14 and PA15 with PA14 being also SWCLK. Now I can't upload code anymore. I read about putting the MCU into bootloader mode by setting BOOT0 to Vdd. But this doesn't wor...

mmensch by Associate II
  • 2400 Views
  • 4 replies
  • 0 kudos

SPI need help

Posted on July 16, 2013 at 05:15 So ive been trying to get the SPI interface working. Here's what i have so far. void SPI_Setup(void) { SPI_InitTypeDef SPI_InitStructure; SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Direction = SPI_Dir...

timothy by Associate II
  • 1586 Views
  • 4 replies
  • 0 kudos

need STM32F0 SPI Slave Tutorial / working example

Posted on August 08, 2013 at 19:23hi all.. i'm already searching for hours, and can not find a working example / tutorial for SPI Slave on STM32F0. Anyone ?thanks before... #need-stm32f0-spi-slave-tutorial

septijo by Associate II
  • 1906 Views
  • 4 replies
  • 0 kudos

Fatal error: Can not connect to J-Link via USB. Session aborted!

Posted on August 07, 2013 at 23:41I have a STM32 Discovery Kit.  I have set up the IAR compiler.  Succesfully compiled code.  However when I try to download the the Discovery Board I get the following message... Wed Aug 07, 2013 14:21:48: Fatal erro...

greg by Associate II
  • 3005 Views
  • 5 replies
  • 0 kudos

STM32F103VET6 ,converts RGB/YCrCb image data to JPEG

Posted on August 07, 2013 at 10:12Can you help me a little bit?My thesis is about writing the code for image compression and decompression on STM32F103VET6. I have a RGB file and my tasks are writing 1 code to convert the RGB to a JPEG and writing 1...

amore by Associate II
  • 2561 Views
  • 4 replies
  • 0 kudos

STM32F4 Discovery + DM-STF4BB + 180 deg.

Posted on August 08, 2013 at 16:42Hi,I've bought those two boards, but for about 20s DM-STF4BB was rotated 180 deg. so +5V and +3V3 goes somewhere where shouldn't. Do you think DM-STF4BB survived?Second question: from where I can download examples f...

zenek by Associate
  • 1878 Views
  • 3 replies
  • 0 kudos

I2C busy flag

Posted on August 05, 2013 at 12:10 Hello, I am trying to connect two boards using I2C. I have already configured one as master but whenever I send the start condition the I2C bus is busy. Maybe I am wrong in the initialization of the GPIO...

edgar by Associate II
  • 2164 Views
  • 4 replies
  • 0 kudos