STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2S Interrupt and Optimisation

Posted on September 10, 2013 at 17:02Hello All. In my app. I have I2S Transmitter with External Clock. I want to test the clock frequency. At clocktest.c I make: [code] volatile u32 clknum; extern volatile u32 SendTmr; void ClockTest(void){      Del...

TFT LCD with FSMC and External RAM

Posted on June 14, 2012 at 10:00Hi all,I'm working on a project with a dumb TFT LCD (320 x 240). I'm trying to display static images (no double buffer). I've been able to display images (in 565 format) that I load on the flash memory and refresh it ...

joembiye by Associate II
  • 5719 Views
  • 10 replies
  • 0 kudos

How to Store Font Table in Flash with GCC?

Posted on July 16, 2012 at 18:26I have a large 5x7 pixel font table that I want to store in flash memory instead of RAM memory. I am using Eclipse with the ARM GCC plugin.I am hoping there is something similar to avr/pgmspace.h but obviously for STM...

USB callback function for STM32-USB-FS-Device library

Posted on September 09, 2013 at 23:32Hi all,I'd like to define a callback function which can be invoked when USB receives something from the host.  Where should I implement this in the STM32-USB-FS-Deivce library?I know that in Atmel ASL I can do so...

USB D+ Pullup with gpio

Posted on October 24, 2012 at 17:13Hello everyone, I have been experiencing an issue with USB recently on which I wouls need some tips. I have an Olimex H103 board running a STM32F103 chip. I have been running my code on it and usb works fine. I hav...

longchair by Associate III
  • 13792 Views
  • 24 replies
  • 4 kudos

System Handler Priority Config on STM32F4

Posted on September 07, 2013 at 14:33I need to change some system handlers interrupts priorities, but I could not find this function NVIC_SystemHandlerPriorityConfig or something. CMSIS 3.20 & STM32F407 MCU. Can anyone help me? #stm32f4 #systemha...

STM32L Discovery USB

Posted on September 06, 2013 at 20:32Hi, first of all, I'm writing a new thread because I couldnt reply to [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32LDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32LDiscovery/STM32L%2...

codium by Associate II
  • 1887 Views
  • 5 replies
  • 0 kudos

STM32VLDiscovery EXTI

Posted on September 08, 2013 at 06:54 My question is probably simple. Can I configure external interrupts triggered by PA10, PA11, PA12 and PA13? Studing the EXTI example I understood something like this: PA0 is connected to EXTI_L...

hprado by Associate II
  • 2531 Views
  • 6 replies
  • 0 kudos

ADC offset error

Posted on September 06, 2013 at 13:49I am using 2 ADC inputs on an STM32F103.  Vref is 2.500V, from a voltage reference. One input is multiplexed via relays from a variety of external analogue signals and works well.  The other is used to monitor th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.