Skip to main content
shivabhardwaj4
Associate
November 11, 2012
Question

USART echo program not working

  • November 11, 2012
  • 3 replies
  • 775 views
Posted on November 11, 2012 at 02:08

Hello,

I am trying to implement a simple USART echo program but am running into communication problems between the discovery board and puTTy. When I transmit a character to the discovery board it does not respond. I have my serial adapters transmit line hooked up to a scope which is outputting an 8 bit value in accordance to the configuration of 4800 baud, 1 stop bit and no parity. However even though i can see a signal being sent to the STM i am not quite sure why it does not echo and send a character back.

 

the code I am currently executing is below

int main(void)

{

 

        RCC_Configuration();  //clock initialize for usart2

        //NVIC_Configuration();

        GPIO_Configuration();//pins 2 and 3 configurationaaa

        init_usart();

        STM_EVAL_LEDInit(LED4);

        STM_EVAL_LEDInit(LED5);

    while(1)

        {

             uint16_t Data;

             

            while(USART_GetITStatus(USART2,USART_IT_RXNE) == RESET) ;

            // STM_EVAL_LEDToggle(LED4);

            Data = USART_ReceiveData(USART2); // Collect Char

            while(USART_GetITStatus(USART2,USART_IT_TXE)== RESET); // wait for empty

               USART_SendData(USART2,Data); // defined in stm32f4xx_usart.h 

  }

}

I have even tried just putting   USART_SendData(USART2,0x61) in the main while loop, but instead of the lower case a i should receive I am seeing an 'O' character in puTTy.

Please help me I dont know where I am going wrong!!!

#use-an-oscilloscope
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    November 11, 2012
    Posted on November 11, 2012 at 06:02

    Please help me I dont know where I am going wrong!!!

    So are we supposed to guess with absolutely NONE of the initialization code that might critically impact the functionality?

    If the baud timing is wrong, I'd look at the value of HSE_VALUE and how that contrasts with actuality.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    pccmd
    Associate II
    November 11, 2012
    Posted on November 11, 2012 at 18:34

    Shiva,

    Please post the specific codes for configuration of USART and GPIO pins set for AF, as well as NVIC. Sometimes one small omission will not generate an build error, but render you entire project dead just the same.

    Andrew Neil
    Super User
    November 12, 2012
    Posted on November 12, 2012 at 11:19

    ''I have even tried just putting   USART_SendData(USART2,0x61) in the main while loop, but instead of the lower case 'a' i should receive I am seeing an 'O' character in puTTy''

    So what does that tell you?

    You said you have an oscilloscope...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.