STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB FS core and HS core simultaineously

Posted on September 06, 2013 at 21:23Since the STM32F407 has 2 USB ports, OTG_FS and OTG_HS, can both ports run at the same time? I want OTG_FS to operate as a host and OTG_HS to operate as a device at the same time.All of the sample code from ST op...

tager by Associate
  • 1162 Views
  • 2 replies
  • 0 kudos

bootloader and atollic

Posted on September 05, 2013 at 17:11Hello,I work on the bootloader IAP_ethernet from ST.I use the TFTP transfer.When I use the image ''Ethernet_IAP_STM3240 \ binary \ STM324xG_EVAL_SysTick.bin'' provided in the example AN3376, it works correctly.Wh...

pcu by Associate II
  • 999 Views
  • 3 replies
  • 0 kudos

ETH_MACFFR.PCF field

Posted on May 19, 2013 at 10:04Quote from Reference ManualBits 7:6 PCF: Pass control framesThese bits control the forwarding of all control frames (including unicast and multicastPAUSE frames). Note that the processing of PAUSE control frames depend...

dimax by Senior
  • 1069 Views
  • 2 replies
  • 0 kudos

Debug - Print GPIOA->BSSR register

Posted on September 07, 2013 at 00:56Hi,How can I print the GPIOA->BSSR register using gdb? I tried to p using the register address but with no success: (gdb) n 67              GPIOC->BSRR = GPIO_Pin_9; (gdb) p/x *(0x40010800 + 0x10) $6 = 0x0 ...

ee06091 by Associate III
  • 1135 Views
  • 5 replies
  • 0 kudos

How can I redefine it ?

Posted on September 06, 2013 at 14:44Guys, I saw these codes, #ifdef USE_STM3210B_EVAL   #define USB_DISCONNECT                    GPIOD     #define USB_DISCONNECT_PIN                GPIO_Pin_9   #define RCC_APB2Periph_GPIO_DISCONNECT    RCC_APB2Per...

usart -> dma fifo error int

Posted on September 05, 2013 at 04:09 Every time I hit my dma int handler I have an error and it looks like the data i'm sending is all screwed up. Any ideas ? Better yet, any direction as to how to solve these issues myself ? There are ints ...

Debug with GDB - Symbols names

Posted on September 06, 2013 at 17:58Hi,It is possible to use symbols names in gdb? per example:p GPIOA->BSRR instead of: p *(0x40020000+0x18) ?Thanks :)

ee06091 by Associate III
  • 731 Views
  • 0 replies
  • 0 kudos

RTC Calibration STM32F205

Posted on September 06, 2013 at 14:32I'm trying to calibrate the difference of 512Hz at the out  where PC13 possess 511.936Hz which causes about 10 seconds per day delay in the RTC. I'm making the form below, I wonder where I'm going wrong, not beca...

acer by Associate II
  • 795 Views
  • 0 replies
  • 0 kudos

Load and execute code from SD card

Posted on September 06, 2013 at 08:37I want to store part of my code on an SD card and execute it whenever a certain event occurs. I've already figured out how to interface with an SD card so the problem now it getting the machine code into RAM and ...

registers editing problem

Posted on September 05, 2013 at 23:34Hi, I work with STM32F100RB chip and i got a little problem with editting registers of some peripheral. I got a problem with edit DMA registers. Even if I use code from DMA example in my project and build it, the...

onbartik by Associate II
  • 1046 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.