cancel
Showing results for 
Search instead for 
Did you mean: 

DataBind error on STM32 forum

Posted on November 09, 2012 at 17:55

Server Error in '/' Application. The control collection cannot be modified during DataBind, Init, Load, PreRender or Unload phases.

Description: An unhandled exception occurred during the execution of the current web request. Please review the stack trace for more information about the error and where it originated in the code.

Exception Details: System.Web.HttpException: The control collection cannot be modified during DataBind, Init, Load, PreRender or Unload phases. Source Error:

 An unhandled exception was generated during the execution of the current web request. Information regarding the origin and location of the exception can be identified using the exception stack trace below.

Stack Trace:

[HttpException (0x80004005): The control collection cannot be modified during DataBind, Init, Load, PreRender or Unload phases.] System.Web.UI.ControlCollection.RemoveAt(Int32 index) +11110720 System.Web.UI.Control.AddedControl(Control control, Int32 index) +11036232 ST.App.MySTCom.Forums.WebParts.CommunitiesAllForums.RunAnonymous() +209 System.Web.UI.Control.EnsureChildControls() +146 System.Web.UI.Control.PreRenderRecursiveInternal() +61 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Page.ProcessRequestMain(Boolean includeStagesBeforeAsyncPoint, Boolean includeStagesAfterAsyncPoint) +3394 

#forum-broken
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on November 09, 2012 at 17:59

Hopefully the database isn't fatally corrupted, but it appears to be melting down.

Suggest posters use the STM32 Discovery forum, as the STM32 forum is currently unreadable for posts made on 9-November-2012.

I've attempted to contact a moderator.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on November 09, 2012 at 18:43

Also noted on the ''Forum related Functionality issues'' forum:

[DEAD LINK /public/STe2ecommunities/e2efeedback/Lists/Functionality%20issues/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/Functionality%20issues/STM32%20Forum%20Server%20Error%20in%20%27%27%20Application&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C1184011A4DEFF4BA0E41441DCAEC568]https://my.st.com/public/STe2ecommunities/e2esupport/Lists/Functionality%20issues/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fe2esupport%2fLists%2fFunctionality%20issues%2fSTM32%20Forum%20Server%20Error%20in%20%27%27%20Application&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C1184011A4DEFF4BA0E41441DCAEC568

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
russdx
Associate II
Posted on November 10, 2012 at 01:22

im greeted with this page on most visits to this forum lol, drives me crazy!!!

Posted on November 12, 2012 at 18:30

[DEAD LINK /public/STe2ecommunities/e2efeedback/Lists/Functionality%20issues/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/Functionality%20issues/STM32%20Forum%20Server%20Error%20in%20%27%27%20Application&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C1184011A4DEFF4BA0E41441DCAEC568&TopicsView=https%3a//my.st.com/public/STe2ecommunities/e2esupport/Lists/Functionality%2520issues/AllItems.aspx&currentviews=23]https://my.st.com/public/STe2ecommunities/e2esupport/Lists/Functionality%20issues/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fe2esupport%2fLists%2fFunctionality%20issues%2fSTM32%20Forum%20Server%20Error%20in%20%27%27%20Application&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C1184011A4DEFF4BA0E41441DCAEC568&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fe2esupport%2FLists%2FFunctionality%2520issues%2FAllItems%2Easpx&currentviews=23

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.