STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Code works differently in debug mode than in real time

Posted on November 26, 2014 at 23:47 Hello. I've got problem regarding STM32L100 (on discovery board). I've switched from Arduino where I enjoy the simplicity of printing data to via UART and delay/millis functions. So, I decided to write my own...

How are you supposed to use HAL_UART_Receive in STM32Cube ?

Posted on November 25, 2014 at 18:52I am implementing a command parser that receives data on a serial port. My need is to read one byte at a time and when I recive a full command I will handle it. I look at the example in STM32Cube_FW_L0_V1.1.0\Proj...

johan2 by Associate II
  • 1967 Views
  • 2 replies
  • 0 kudos

TIM_ICPOLARITY_BOTHEDGE Input capture in STM32L

Posted on November 28, 2014 at 19:24Hello Guys,I´m developing an application with STM32L and I would like to use TIM2 Input capture with TIM_ICPOLARITY_BOTHEDGE.When the interrupt occurs...Is there a way of knowing which Polarity has been detected?M...

gerardo by Associate II
  • 2977 Views
  • 7 replies
  • 0 kudos

can t compile ARM_MATH.h

Posted on November 27, 2014 at 21:35Hi, I am using coide and arm gcc compiler to build my projects.When i try to compile arm_math.h ,i got those  errors a LOT of times.unknown type name '__INLINE expected '=', ',', ';', 'asm' or '__attribute__' befo...

d4ng3r09 by Associate II
  • 1174 Views
  • 3 replies
  • 0 kudos

DAC waveform generation with DMA not working

Posted on November 27, 2014 at 15:45I am using the STM32L Discovery Board (STML152RB chip on board). The IDE is Emblocks. I was trying to generate a sawtooth wave signal using DAC and DMA but it does not work. I was able to make the same program wit...

STM32 Digital Photo Frame

Posted on November 28, 2014 at 14:22An STM32F103 Based Digital Photo Frame utilizing uCGUI Graphics Framework with source code. This is a good tutorial if you want to learn using Graphics Framework uCGUI from Micrum, FAT FS Embedded File System by C...

What is CPRI on the HD STM32L1?

Posted on November 26, 2014 at 18:05Hello, looking at the datasheet of the HD STM32L1 devices, A CPRI function is listed in table 10. However I didn't find any information on the web and on the ST website about that function. Any information welcome...

STM32F407VG Eval Board

Posted on November 27, 2014 at 14:02Hi,                    I am a beginner in the ARM Cortex Series and so far I could able to run some simple examples on my STM32F407VG Board. Currently I am working with a project where I need to establish the comm...

jayakanth by Associate II
  • 2229 Views
  • 5 replies
  • 0 kudos

Delete (mass erase) flash bank 2 on STM32F429II

Posted on November 27, 2014 at 14:06 I have a STM32F429II with 2 x 1MB flash memories. It supports Read-While-Write on the flash banks. I have written code to write/read to the flash memory bank 2 and my application is on the flash bank 1. I hav...

phb by Associate II
  • 1616 Views
  • 1 replies
  • 0 kudos

STM32F303RE: linker file for GNU based tool chain

Posted on October 17, 2014 at 17:05Hi,I have a c++ application that is running on STM32F303RC (256 K flash).I want to use this same application on the new STM32F303RE (512 K flash).I modify the linker file as follow:/* Entry Point */ENTRY(Reset_Hand...