Posted on October 02, 2014 at 21:51Hello, I am having hard time to figure this out. in the data sheet it is mentioned that the STM32F407 works at a maximum clock of 168 Mhz, but using any module timer, PWM or any other the clock is divided by ...
Posted on August 14, 2014 at 06:12Hello friends, I have a program to send data at very high speed over the USB (Msps). I want to use the DMA to handle this. Can anyone suggest me what should be my line of action or some examples would be g...
Posted on August 13, 2014 at 07:21Hello, I am generating a signal which goes to output of the DAC, but unfortunately when I use the PWM module of the system the PWM signal frequency distorts the signal generated by the DAC.Can anyone tell me...
Posted on August 12, 2014 at 19:18Hello, Can anyone help me with the an example of SPI communication between two STM32F4 Discovery Board. I have an example but with the HAL API which I dont want to use right now.RegardsSameer #stm32 #spi
Posted on August 12, 2014 at 00:35Hello I just migrated from STM32F407 to STM32F429, How DO I change the system clock from 168Mhz to 180Mhz. I modified the system_stm32f4xx.c file, but I cant change it. Please let me know.Thanks #clock #stm32f429
Posted on August 09, 2014 at 01:32Thanks again, I am using the STM32F4 discovery board. I am using unbuffered for both the DACs. I am just probing at the pins no buffered input or output going to any pin.