Posted on May 05, 2014 at 12:44HI,It is possible to use the graphical library from ST to create a graphical application with STM32F407? What about the LCD ?Best Regards ,
Posted on April 20, 2014 at 16:45Hi,It is possible to receive data via CAN and send them via HDMI using STM32F4 ? If yes , How can I do ? Thanks.Regards ,
Posted on May 06, 2014 at 10:49Sorry for this question , I'm beginner with STM32 . I've found the package stm32f4cube and i'used BSP drivers . Now , If I want save the image of the screen in order to send them to another device . How can I do ?
Posted on May 05, 2014 at 18:45I want to display an image and a data (example temperature). For graphical application , I 've found STM32F429I and the tool embedded graphic editor. So , how can I process ? Is there any sample project of graphical ...