STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[solved] works FSMC correct on stm32f407vg ?

Posted on November 25, 2014 at 11:33 Hi. All! I want to use FSMC module, but I'm not sure that it settings correct. There is write operation on a picture. I see multiple NWE activation. And sometime it release NEx together NWE (should be NWE...

0690X00000602yqQAA.jpg
t2399 by Associate II
  • 5113 Views
  • 8 replies
  • 0 kudos

TEC CAN error instantly full

Posted on November 27, 2014 at 20:31Hi all!   In what cases will the Transmit Error Counter register jump from 0 to 0xF8? I am debugging this CAN transmission sequence, and after the Transmit request is set, the next step in debug will show a full E...

zamolan by Associate II
  • 1239 Views
  • 0 replies
  • 0 kudos

Run code from SDRAM with STM32F4 (e.g. STM32F229)

Posted on November 18, 2014 at 14:14Hello, we are considering to use the STM32F4, probably the STM32F429 or STM32F427. For our application we would need to run the program from SDRAM. I was looking around for application notes, but could not find s...

stcom9 by Associate II
  • 6668 Views
  • 13 replies
  • 0 kudos

Compilation with files from STM32CubeF4 on linux

Posted on September 06, 2014 at 09:02Hello all. I just got a STM32F429-DISCO board and compiled my first successful program. I'm working under linux compiling with the GNU toolchain for ARM. In order to be able to compile my program, I had to modify...

pgarista by Associate
  • 1239 Views
  • 3 replies
  • 0 kudos

STM32F4 timer (Prescaler Value)

Posted on January 24, 2013 at 03:46Hi, I have just saw a program about a interrupt time. The program can let the LED on and off in a specified period. But I have some question about the prescaler value, can anyone help me to understand the prescale ...

kazafwing by Associate II
  • 6206 Views
  • 13 replies
  • 1 kudos

RTC initialization

Posted on November 29, 2011 at 17:56 Our design is made with  a STM32F207ZG microcontroller and we have some problems with the RTC peripheral. We have an external 32.768 kHz oscillator (LSE).         Using the ST library, the initialization of the R...

math.h not in the firmware

Posted on November 27, 2014 at 11:15Hi,I am currently using the dsp library .I noticed that it need math.h library to run correctly.Unfortunately, i couldn't find it on the internet.Does somebody have a link?

d4ng3r09 by Associate II
  • 1025 Views
  • 1 replies
  • 0 kudos

STM32F4 & Ethernet configuration (RMII)

Posted on November 27, 2014 at 11:25Good day,Given you use the RMII interface to the STM32F4 MCU does anybody know what the CR (clock range) needs to be configured to?  The RMA is not clear if the clock range configuration is for the MII interface o...

truhann by Associate II
  • 1500 Views
  • 1 replies
  • 0 kudos

timer Dma burst transfer

Posted on November 27, 2014 at 10:48 I found an example in the stm firmware. It is TIM DMA Burst. The configuration code is as in this link https://github.com/devthrash/STM32F4-workarea/blob/master/Project/STM32F4xx_StdPeriph_Examples/TIM/TIM...

Regarding STM32F207 Timers ISR

Posted on November 26, 2014 at 11:11Hi, I am very new to 32 bit micro-controllers.I am using STM32f207VG controller.I want to use Timer2 to generate Interrupt every 1 ms.Timer clock is set to 36MHz. I have written the following code for timer ISR.My...

er by Associate II
  • 1499 Views
  • 4 replies
  • 0 kudos