cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 clock Jitter on TIM4

fernando
Associate II
Posted on April 02, 2014 at 08:56

Hello everyone, I'm using STM32F100V8 and I configured TIM4 to generate a square wave (for uart sw). The TIM4 is so configured and should have the highest priority: 

  TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); 

  TIM_TimeBaseStructure.TIM_Period = 1; 

  TIM_TimeBaseStructure.TIM_Prescaler = 405;

  TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; 

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; 

  TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);

  TIM_ITConfig(TIM4, TIM_IT_Update , ENABLE);

  NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);

  NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQChannel;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);  

Inside the ISR of TIM4 i toggle a MCU line and my scope show me that the clock has a very high jitter; Could someone give me some suggestion to make te clock more stable ?

 Here attached an image from my scope acquired on a long time with infinite persistence time 

#stm32-clock-jitter-tim4
This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
waclawek.jan
Super User
Posted on April 02, 2014 at 09:47

Don't toggle the output pin ''manually'' in the ISR. Rather, use one of the output compare channels and set it to change state in the ''future'' as needed.

A completely different approach may be to use the timer as trigger for DMA transferring from a prepared array in RAM to GPIO.

JW

fernando
Associate II
Posted on April 02, 2014 at 11:37

Thanks for the reply. Could you please explain me why I can't toggle the pin manually inside the ISR ? 

waclawek.jan
Super User
Posted on April 02, 2014 at 12:00

... to avoid the jitter caused by the zillions of factors causing variable latency of the ISR....

Mind, this is NOT a microcontroller. It's a SoC with relatively loosely (as far as timing goes) coupled modules.

JW

Posted on April 02, 2014 at 15:42

Could you please explain me why I can't toggle the pin manually inside the ISR ? 

You can, but it's the stupid plan, the TIM peripheral is capable of toggling pins on a hard time line, or generating pulses, etc directly. If you do it in software you get to see all the latency and variability in the servicing.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
gordon2399
Associate II
Posted on May 05, 2014 at 22:28

I have the similar problem.  I am relying on the timer to provide constant timing for ADC sampling.  SPI command is used to read the ADC.  The CS pin negative edge starts the acquisition.  I manually set and reset the CS pin in the interrupt routine, but the CS pin has high jitter.  That adds lots of noise to my FFT plot.  Is there a way to minimize the jitter?  I am using STM32F415

Posted on May 06, 2014 at 02:10

You could presumably drive the CS pin as a TIM PWM signal, you could cause the pin to go low for a prescribed period, one into which you'd then perform your SPI transaction, starting it in the CCx interrupt

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
gordon2399
Associate II
Posted on May 06, 2014 at 21:20

Sorry, I was not clear in my explanation.  For the ADC that I use, both CS and SCLK must not have jitter.  The ADC actually starts the acquisition at the fourth rising edge of SCLK.  I understand your comment about using the PWM output as the CS signal, but that doesn't solve the jitter problem for SCLK.

Posted on May 06, 2014 at 21:50

Perhaps you can use a TIM triggered DMA into the SPI peripheral?

Other than that you might want to get the hardware sequencing handled in a CPLD?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..