cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK/V2 and Win7 64-bit

pyoung
Associate
Posted on August 21, 2012 at 22:28

Has anyone tried using the ST-LINK CLI.exe in windows 64-bit? Is there a way to make win7 run it as 32-bit?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on August 21, 2012 at 22:37

Windows XP Mode?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
leon355
Associate II
Posted on September 05, 2012 at 16:57

I'm using Win7 x64 with STM32 ST-LINK Utility.exe without any problems.

lmullane
Associate II
Posted on June 26, 2013 at 15:11

On Windows 64bit I can get the STM32 ST-LINK Utility.exe to work.

However as Phil said in first post I can't get the ST-LINK CLI.exe to work 

Is it compatible with Windows 64 Bit?

Posted on June 26, 2013 at 16:40

Well he doesn't say it doesn't work, although that might be the inference. Others have suggested it is workable.

Useful information for ST might be what version of the tool/driver is in play, and what SP your Win 7 x64 is using. This is primarily a user forum, with some ST participation in recent weeks.

There are always going to be a subset of tools that won't work in Win7 x64, be they tied to old/obsolete drivers, or 16-bit DOS/Windows code, etc. It might be useful for you to discover Virtual PC (XP-Mode) or VirtualBox.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
lmullane
Associate II
Posted on July 01, 2013 at 13:41

Removed drivers, downloaded and installed latest drivers, and now the ST-LINK CLI.exe works on my 64 Bit Windows 7, so all good again :)

anoirnechi
Associate II
Posted on May 06, 2014 at 23:41

Hi

i've just bought an stm32f407 ..... when i connect it to my computer ... this last, dont recognize it so i've installed the stlink driver, but the problem is still the same .... can someone help me please.

thank you
Posted on May 07, 2014 at 01:27

i've just bought an stm32f407 ..... when i connect it to my computer ... this last, dont recognize it so i've installed the stlink driver, but the problem is still the same .... can someone help me please.

Yeah, not really much meat there.

So a Windows 7 x64 machine, and a STM32F4-DISCO? What version of the driver?

This driver?

http://www.st.com/web/catalog/tools/FM147/SC1887/PF258167

What does Device Manager have to say about the driver and the board?

Can the ST-LINK Utilities see it? What version of firmware? Can you upgrade it to V17?

http://www.st.com/web/catalog/tools/FM147/SC1887/PF258168

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
anoirnechi
Associate II
Posted on May 07, 2014 at 18:25

 Windows 7 x64 machine

i've already installed the driver that you gaved me 

STlink utilities can't see the board

the device manager can't install the driver of the board .... every time i connect it, i see a message of '' unknown device''

i'm really confused.

Posted on May 07, 2014 at 18:51

Which connector are you using?

Do you have any setting precluding the use of unsigned drivers, or USB devices? Does this work on any other machines? Is this a corporate machine, what does IT say?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..