STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

read/write multiple files using fatfs

Posted on March 14, 2015 at 02:59i require to open multiple files simultaneously and, read and write multiple files using stm32f4 and fatFs , as a test i used f_open with 4 different file names and file pointers but only two files got created in car...

scholar by Associate II
  • 3248 Views
  • 1 replies
  • 0 kudos

FIR filtering on STM32F4

Posted on March 12, 2015 at 09:36Hi,in my application, I need to make signal filtering using digital filters.I take ARM's DSP library and fir example, but it is not so useful for me, because there are samples stored in memory already and they are us...

tm3341 by Associate II
  • 2209 Views
  • 4 replies
  • 0 kudos

STM32F105 SPI2 issue

Posted on March 13, 2015 at 19:06Hello all, I faced problems with SPI2. First I interfaced a graphic LCD on SPI bus and could not get to working properly, though it works well on an Atmel 8 bit controller. Spent more than 3 weeks without much luck. ...

nps by Associate II
  • 1332 Views
  • 5 replies
  • 0 kudos

DMA double buffer with STM32CubeMX

Posted on November 09, 2014 at 23:37I want to use DMA with double buffer. STM32CubeMX provides options for normal and circular buffer. Should I select circular buffer and then modify the source or is it better to wait for the next version of STM32Cu...

sdim by Associate III
  • 3698 Views
  • 4 replies
  • 2 kudos

Invalid clock pulse on I2C

Posted on March 11, 2015 at 09:04 I am using microcontroller STM32F On reading EEPROM operation with I2C microcontroller gives 7 clock pulses instead required 9. There is fragment of transmitting on picture. When this cause o...

0690X00000605F0QAI.png
sdianoff by Associate II
  • 2845 Views
  • 3 replies
  • 0 kudos

STM32F207 and STULPI01B Registers

Posted on August 21, 2013 at 17:05Hello. I have been searching the forums and cannot find an answer, hence I am starting a discussion here. I have been using the STM3220G-EVAL board and the HS USB onboard PHY (obsolete NXP device). I have since crea...

ckern by Associate II
  • 696 Views
  • 1 replies
  • 0 kudos

STM32L1 SPI throughput

Posted on March 13, 2015 at 16:17Hello, I'm running an STM32L151 at 32MHz and SPI BaudRate = fPCLK / 4. The device is an SPI Master, and tries to read a Slave as fast as possible. I'm using DMA TX and RX to speed up things. I can see the SPI clock r...

Kuikui by Associate III
  • 706 Views
  • 0 replies
  • 0 kudos

USB CDC state detection

Posted on October 04, 2013 at 17:53Hi All, i'm using STM32F407 in USB CDC mode, i'm having issue when i'm sending bytes from STM to PC, client application on PC is minicom, issue is when i close minicom and STM runs into ''frozen'' state until i...

STM32F3: Back to Read Protect level 0

Posted on March 12, 2015 at 14:27eg:The 10 first pages of Flash are write protected.The read protect level 1 is activated.What's happen when going back to level 0 ?According Reference manual, a mass erase is done but what's happen to the write prote...