STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 custom bootloader with encryption support

Posted on March 11, 2015 at 17:24Hello,     I am trying to develop a product with STM32F407 processor that must be firmware upgradeable in the field. The problem that I am thinking of is that somebody could easily make the same hw design of the boar...

Band Pass Filter STM32F429i discovery kit

Posted on March 13, 2015 at 09:32I am new to DSP. I have done fft and filtering using scilab tools. now same thing i want to do on stm32f429i discovery kit. I need Band Pass Filter (0.5 to 5Hz) in STM32F429i discovery kit. we dont have any tools whe...

lokesh by Associate II
  • 800 Views
  • 0 replies
  • 0 kudos

The exact mean of ''USE_RTOS''

Posted on March 13, 2015 at 04:03In the CubeMX generated code, I found this macro ''USE_RTOS'', in the implementation of HAL_LOCK macro. And the comment '' USE_RTOS should be 0 in the current HAL release ''. But now I'm using FreeRTOS. So I need to ...

lo_529 by Associate III
  • 895 Views
  • 0 replies
  • 0 kudos

Spurious SAR trigger by Disabled timer

Posted on March 11, 2015 at 14:48I'm setting up a process where a regular group of SAR conversions will be triggered by a timer. The SAR is configured to use DMA to transfer that data into a buffer. The buffer memory is actually organized into two b...

iumez by Associate II
  • 3375 Views
  • 8 replies
  • 0 kudos

[SOLVED] STM32F205 DAC Speed

Posted on July 04, 2014 at 10:20I am using the code from the DAC with DMA example in the Standard Peripheral Library V1.1.0 to produce a sine wave. The updates seem to occur about every 4.5us. Is it possible to significantly increase the update spee...

sm23 by Associate II
  • 2317 Views
  • 5 replies
  • 0 kudos

STM32CubeMX freeRTOS

Posted on July 21, 2014 at 19:34Hi ,1. How Can i Find which version of freeRTOS the STM32CubeMX add to the project ?2. I don't Know if this the right place to ask , but does freeRTOS fully support     CMSIS-RTOS API ?  Thanks .

eyals111 by Associate II
  • 1683 Views
  • 2 replies
  • 0 kudos

SPI problem NucleoF401<->TI Launchpad

Posted on March 11, 2015 at 23:38 Hello, I am having a little problem with my SPI between the nucleo board and the TI cc3200 launchpad. I have been using the SPI communication without any problem under the following configuration ...

salman by Associate II
  • 1401 Views
  • 2 replies
  • 0 kudos

I2C_FLAG_BUSY problem

Posted on July 10, 2014 at 10:49Good morning,  I have some problems on I2C bus on STM32F1 micro. I have 8 prototipes board (all with the some mounting). 4 of those works fine and I can read and write the EEPROM on board (a 24xx series standard memor...

stefano23 by Associate II
  • 2189 Views
  • 2 replies
  • 0 kudos