User Activity

Posted on September 25, 2015 at 11:57I have a STM32F2 with OTG periphery and STM32 USB Host Device library in FS host mode. The other end is STM32F4 OTG FS with the same library but in Device mode as VCP. When I connect the device to the Host, it is...
Posted on August 25, 2014 at 10:55I am using STM32L100 MCU with STLink v2 for debug and flash/eeprom programming thru SWD. This is a device with soldered battery - i.e. it is permanently supplied. If I want to reprogram e.g. EEPROM I connect STLink ...
Posted on July 18, 2014 at 15:46I would like to set a Vcore voltage range to 1.5V and then back to default 1.8V on STM32L1xx for some code execution. I did not found anywhere the correct procedure, what everything has to be change, but generally it ...