Skip to main content
chris239955_stm1_stmicro_com
Associate II
August 25, 2014
Question

STM32F205 DMA Problem

  • August 25, 2014
  • 2 replies
  • 722 views
Posted on August 25, 2014 at 09:18

Hello,

I am trying to use DMA to transfer data from a buffer in RAM to a GPIO BSRR port triggered by a timer.  Due to the way the hardware is laid out I am committed to using TIM5 as the trigger.  The DMA trigger is TIM5 Update on channel 6 stream 0 of DMA1.  When I run the software the Number of Data decrements by 1 but the transfer error flag is set and the stream enable bit is reset.  If I change the stream to use TIM1 Update channel 6 stream 5 on DMA2 everything works as expected.  I cannot go over to using TIM1 in the application due to hardware constraints.

Here is the code used to configure the DMA channel

  DMAInit.DMA_Channel = DMA_Channel_6;

  DMAInit.DMA_Memory0BaseAddr = (uint32_t)(&LineCounter[0]);

  DMAInit.DMA_BufferSize = 15;  

  DMAInit.DMA_PeripheralBaseAddr = (uint32_t)&(GPIOC->BSRRL);   

  DMAInit.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;

  DMAInit.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;

  DMAInit.DMA_Priority = DMA_Priority_VeryHigh;

 

  DMA_Init(DMA1_Stream0, &DMAInit); 

Before enabling the timer the registers of the DMA1 stream 0 are

CR   0x0C035541

NDTR 0x0000000F

PAR  0x40020818

M0AR 0x200001E8

M1AR 0x00000000

FCR  0x00000008

And after

CR   0x0C035540

NDTR 0x0000000E

PAR  0x40020818

M0AR 0x200001E8

M1AR 0x00000000

FCR  0x00000020

and LISR now reads 0x00000008

Why does it work on DMA2 and not DMA1?

What is causing this problem and how is it fixed?

Thanks,

Chris
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    August 25, 2014
    Posted on August 25, 2014 at 13:38

    Why does it work on DMA2 and not DMA1? What is causing this problem and how is it fixed?

    Only DMA2 supports memory-to-memory? GPIO on AHB is not a Peripheral on APB1?

    The initialization looks a bit spartan, can you use TIM8

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    chris239955_stm1_stmicro_com
    Associate II
    August 25, 2014
    Posted on August 25, 2014 at 14:29

    Using TIM8 appears to be the only workable solution.  The diagram I was looking at was ambiguous and I thought it suggested GPIO was accessible on both DMA channels