STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 TIM PWM on CH2N only

Posted on July 15, 2015 at 12:29Hello,I have configured only PB0 (TIM1_CH2N) for PWM output, but I can't get any signal from the pin. code looks like this:  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO | RCC_APB2Periph_TIM1, ENA...

How to sprintf an uint32_t value

Posted on July 16, 2015 at 11:43 Hello everybody, Amateur question: I search for a long time how to sprintf a 32bit value in a string. If I use sprintf (string_to_write, ''%u'' , uint32_value); The value is cropped as a 16 bit...

STM32F7 UART problem

Posted on July 16, 2015 at 03:57 I'm using the HAL drivers for the first time and I'm trying to implement the UART protocol. I used the stm32f74g... examples for the UART and copied part of the uart-polling example. The problem I get is t...

pedro by Associate II
  • 1163 Views
  • 1 replies
  • 0 kudos

ST link/STM32F4 Programming other Microcontroller

Posted on July 15, 2015 at 13:15Hi there, I'm going to ask quiet an odd question , is it possible to program an other microcontroller (a pic) using an stm32f4 disco or st link in general. I hope someone can answer me.Many thankx !

monta by Associate II
  • 2596 Views
  • 2 replies
  • 0 kudos

STM32F302 DMA to GPIO

Posted on July 09, 2015 at 22:17Hi All,I'm trying to drive some WS2812 LEDs which require a (400ns high + 800ns low) or (800ns high + 400ns low) signal to indicate a 1 or a 0.So esentially I'm trying to take an array of data and output it directly t...

daniel2 by Associate II
  • 2511 Views
  • 8 replies
  • 0 kudos

STM32F4Disovery - New to embedded programming

Posted on July 15, 2015 at 09:22I have recently got my hands on an STM32F4Disovery board for one of my project requirements. I am supposed to use it with a transceiver and be able to transmit packet. Although I have done a bit of programming, it is ...

sommer by Associate II
  • 642 Views
  • 1 replies
  • 0 kudos

STM32F446 HAL RCC PLLR bug

Posted on July 10, 2015 at 20:59Hello ST developers,I still don't know why I switched to HAL drivers (probably because there is no STD drivers for F7 lines) but I read MANY, MANY bugs in HAL library for F4 and after starting developing generic libra...

tm3341 by Associate II
  • 918 Views
  • 1 replies
  • 0 kudos