STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 I2C Example code

Posted on July 26, 2013 at 04:06I have been trying to make a slave I2C device communicate with my STM32F0 board, with no success. Can anyone give me an example code to config, init and send and receive data through the I2C bus.

STM32 deep sleep pin voltage

Posted on June 11, 2016 at 12:51 I am  using STM32L100This is put into deep sleep so pins are set to inputI am using FET to control power to external devices.  this is connected to PB9  pulled down by 100k resistor. I find that the pin has a voltage...

Flash reading, if MCU is read protected

Posted on June 09, 2016 at 22:16Hi.When read protection level 1 is applied to MCU, is it possible to read flash content somehow?I would like to store CPU status register, PC and some other variables into flash in case of hard fault. But MCU was read...

matic by Associate III
  • 1933 Views
  • 3 replies
  • 0 kudos

CubeMX 4.15.0 - SDMMC clock - bug report

Posted on May 30, 2016 at 20:10I tried to migrate from STM32CubeMX 4.14.0 to 4.15.0 and from STM32CubeF7 1.3.1 to 1.4.0. I found some bug in CubeMX 4.15.0. It is not possible to set the clock for SDMMC using CubeMX. My controller is STM32F746ZGT6, s...

[SOLVED] STM32F103 Generating PWM with TIM4

Posted on June 08, 2016 at 20:10 Hello everyone, I started with STM32F103 two days ago and I need to generate a PWM on GPIOB pin6 using TIM4. I need a PWM of period 20ms with a 1us precision (System Clock is set to 72 MHz) I have...

cyril2 by Associate
  • 3685 Views
  • 3 replies
  • 0 kudos

Migration STM32CubeMX v4.14.0 to v4.15.0 fails!!

Posted on June 06, 2016 at 08:32When i try to migrate CubeMX v4.14.0 to v4.15.0 i get a failure every time! This happens when i use either the green arrow pointing down in the main menu or the Help -> Install new libraries option. The program always...

0690X00000602VIQAY.jpg

DFU standalone doesn't work

Posted on June 10, 2016 at 12:29 I use IAR EW 7.1, HAL driver and STM3210E_EVAL. I would use the application DFU andlike user application CDC_standalone. I've used like configuration for CDC_standalone #define VECT_TAB_OFFSET 0x7000 and...

vbruno1 by Associate III
  • 1054 Views
  • 1 replies
  • 0 kudos

Feature request Stm32CubeMX : Named SPI and I2C buses

Posted on June 08, 2016 at 11:58Hi,I use STM32CubeMX daily to create and modify projects. I really like the way the tool has been improving (e.g. now putting the pin names in a header file for use in the project). An issue I find is that the STM32 d...

cgrant by Associate
  • 1153 Views
  • 2 replies
  • 0 kudos