STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 FMC SRAM problems

Posted on June 02, 2016 at 15:24Hi All,The device is being used STM32F746BGTX.Set as follows.  FMC_NORSRAM_TimingTypeDef Timing;  /** Perform the SRAM1 memory initialization sequence  */  hsram1.Instance = FMC_NORSRAM_DEVICE;  hsram1.Extended = FMC_...

sim20 by Associate II
  • 4355 Views
  • 9 replies
  • 0 kudos

External PSRAM and FSMC on STM32F76xxx

Posted on June 13, 2016 at 09:37Hi,I need help enabling page read mode in external memory  http://www.issi.com/WW/pdf/66-67WVE4M16EALL-BLL-CLL.pdf.This external memory supports faster asynchronous page reads (shown on page 10) but Ican not find need...

ales by Associate
  • 1324 Views
  • 1 replies
  • 0 kudos

Switching STM32F103 GPIO From Input and Output

Posted on June 13, 2016 at 02:06 Very new to STM32 development and am not an engineer, so apologies for what is likely a very silly question. I'm attempting to use an STM32F103 as a programmable replacement for a game cartridge ROM. When ...

STM32F030 multiple UART problems

Posted on June 11, 2016 at 18:07  The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F7 Mem-to-Mem DMA problems

Posted on June 09, 2016 at 20:36 Hi all, I'm trying to setup a very simple Memory to Memory DMA transfer. DMA status registers report that the transfer completes OK, but the memory contents is not transferred. Can anyone see why...

mwp by Senior
  • 1648 Views
  • 3 replies
  • 0 kudos

two EXTI conflict

Posted on June 12, 2016 at 08:51Hi!Im trying to use two EXTI on PE2 and PE3 pins simultaneously. Two push bottons are connected to these two pins with a pull-up resistor and a capacitor filter prohibitting debounce phenomenon. As shown in the code b...

Set Internal trigger connections to TIM2 in STM32CubeMX

Posted on June 08, 2016 at 05:37By the DM00032020 Reference Manual, when TIM2 is used as slave, it's trigger source can be IRT0 from TIM1, ITR1 from TIM8, ITR2 from TIM3, IRT3 from TIM4. But now, when choose trigger source ITR1 in the 'pinout' card....

some basic doubts from CubeMX

Posted on June 11, 2016 at 20:40Hi,i m using 103RB nucleo board and keil compiler. I have configured code for one interrupt. CubeMX is generated code for handler also. But i m not able to find out how handler function is linked to vector address..I ...

SS.Sagar by Associate III
  • 768 Views
  • 1 replies
  • 0 kudos

pwm generation problem stm32f303

Posted on June 11, 2016 at 01:55 Hi to all, I'm giuseppe and I'm new here, I've a big problem with the generation of pwm signal, in the code below i'm trying to create a pwm of 50% duty cycle in port PA0, the pwm would be of a period of 1s, s...