Hello to all.I'm trying to setup the STM32F746-Discovery board for audio transmission.For the audio transmission it is important to use double buffer mode.I'm using the HAL and the stm32746g_discovery_audio.c and wm8994.c filesThe LISR register signa...
Posted on January 07, 2016 at 14:02
Hello all,
I obsarvate an problem with the DMA in STM32F2.
I am using the STM322xG-Eval Board for the development.
The firmware streams data from SRAM to I²S by DMA. I also use in the same firmware...
Posted on January 07, 2016 at 21:51
Hello Jack,
thank you for your answer.
As you can see in the first pic in my previous post, there is only the HTIF flag set.
The ISR Routine isn't called if the failure occurs.
I also check in ...