cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link Upgrade

mbmail4
Associate II
Posted on January 07, 2016 at 10:24

Hi All.

I'm new to this forum, and new to STM32, and have come across a problem.

I'm using Atollic lite and an old STM32VLDiscovery board I purchased a while ago.

When I try to start a debug session Atollic gives an error:

Error in initializing ST-Link device.

Reason: (-6) ST-Link firmware upgrade required.

Please upgrade the ST-Link firmware using the upgrade tool. Reconnect ST-LINK and click OK.

When I try to upgrade the firmware the upgrade utility tells me, that ST-Link is not in DFU mode and needs restarting. No matter what I do I cant get it to upgrade. Can anyone help on this?

Thanks

Martin

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on January 07, 2016 at 11:37

Try pressing or holding the RESET button while doing so.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mbmail4
Associate II
Posted on January 08, 2016 at 00:35

Thanks for your reply. I finally worked it out. You have to unplug and re plug the discovery board after you select the firmware upgrade option. The reset switch is connected to the target, not the programmer, so re starting is the same as resetting. I'm sure its documented somewhere.

martin