cancel
Showing results for 
Search instead for 
Did you mean: 

Windows-10 update breaks STLink Utillity

Andrew Neil
Super User
Posted on January 07, 2016 at 15:07

A colleague updated the HP Win-8 Laptop he was using to Win-10.

The STLink Utility v2.7.0 had been working prior to the update, but would not see any STLink after the update (2 dongles & a genuine STLink were tried).

The Windows Device Manager showed the STLink as present but said driver not recognised (or something).

Uninstalling & re-installing the STLink Utility v2.7.0 (from the original installer download) fixed it.

#windows-10-is-a-virus
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on January 07, 2016 at 19:02

Others have reported a failure, Win8 compatibility mode reportedly fixed the issue.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..