STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IAP Go to infinite loop when Hard Fault

Posted on June 08, 2016 at 16:57STM3210E_EVAL on board after erasing the flash, I installed IAP application as STM32Cube_FW_F1_V1.3.0.Running the IAP program without having loaded any user application code, the micro goes hard fault. I think it is n...

vbruno1 by Associate III
  • 1999 Views
  • 6 replies
  • 0 kudos

Facing problem in GPIO configuration

Posted on June 08, 2016 at 19:27Hi,I m configuring GPIO port for OUTPUT. but, i m not able to configure it propely.Following is my implmentation which is not working. GPIOC->CRL |= 0x00000001<<20; // GPIOC-5th GPIOC->CRL |= 0x00000001<<24; // GPIOC-...

SS.Sagar by Associate III
  • 1206 Views
  • 3 replies
  • 0 kudos

STM32F429 SPI 5 Problem - Clock

Posted on June 08, 2016 at 13:09Hi all,I am trying to read the onboard Gyro on STM32F4 discovery board. As mentioned in datasheets, Gyro(L3GD20) is conneted to SPI 5. I have configured everything, but I am not able to generate the required clock  on...

maharaj by Associate II
  • 1121 Views
  • 1 replies
  • 0 kudos

STM32CubeMX and BUG in UART_DMATransmitCplt

Posted on November 02, 2015 at 12:53STM32CubeMX V4.11STM32Cube FW_F4 V1.9.0/**  ******************************************************************************  * @file    stm32f4xx_hal_uart.c  * @author  MCD Application Team  * @version V1.4.1  * @d...

When to use DMA on USART

Posted on June 09, 2016 at 11:29Hi,I'm fairly new to micros with DMA and am wondering when to use the DMA to create a cyclic buffer.Background...I'm looking to update some working but un-maintainable drivers, eventually I'll be sorting I2C, ADC, SPI...

PolarSSL

Posted on June 07, 2016 at 16:48Hello, is the Polar SSL (mbed TLS) Stack running without RTOS ? Thanks in advance Michael

STM32F103 USART - PC receives wrong data

Posted on June 08, 2016 at 11:45 Hi guys, I've implemented the code to send data from STM32f103 to PC with USART interface, but the data that I receive are wrong. This is the code that I've implemented : void RCC_Configuration(...

0690X0000060395QAA.jpg
verdano by Associate II
  • 7029 Views
  • 16 replies
  • 0 kudos

FW repo source files incomplete?

Posted on June 08, 2016 at 08:08I have been trying, with limited success, to create a project in CubeMX and then import the example application files from LwIP HTTP server app so I can start to find a solution for my specific tasks.  In the process ...

SIM800 with stm32f334

Posted on June 09, 2016 at 02:21Hi all;I am trying to send sms using sim800l module with stm32f334&sharpinclude ''mbed.h''&sharpinclude <string>Serial pc(SERIAL_TX, SERIAL_RX); // pc comunicationSerial SIM900(PA_9, PA_10);   //tx, rx SIM 900string r...