STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Real breakpoints with ADC and interesting phenomenon

Posted on August 08, 2017 at 14:52I'm using STM32F103CB to convert the analog outputs from three polar hall sensors arranged circularly, a magnetic actuator rotates in the center, but I get the voltage value with strange breakpoints, and these happe...

0690X00000607yHQAQ.png 0690X00000603zuQAA.jpg 0690X000006040EQAQ.jpg 0690X00000603zzQAA.jpg

STLINK Utility V3.9.0 Installer

Posted on August 09, 2017 at 04:55Where can I get the old release of STLINK Utility? The latest version (V4.0.0) is failing on me. I need the V3.9.0. Anybody has the installer for windows 7?

STM32(F4) register programming

Posted on August 08, 2017 at 18:56Hi,I would like to programm my mcu (stm32f4) directly with the reference manual. Are there some examples from ST to see how it is done? I would need for the start examples of: I'C and GPIO.Hope you could help me,tha...

uli stone by Associate II
  • 3150 Views
  • 6 replies
  • 0 kudos

STM32CubeMX bug - can't select AF on PH6

Posted on August 09, 2017 at 03:39STM32CubeMX 4.22.0, F7 cube 1.7, stm32f769i-discoveryI want a 32 bit timer with pwm capture on the arduino headers. Attempting to select TIM2_CH1 on  PH6 fails. In the application, it just puts the ball to reset mod...

0690X00000607l8QAA.png

Resolved! STM32CUBEMX feature request

Posted on August 08, 2017 at 22:50Hi, I currently have a CUBEMX project for a STM32F7 LQFP100 chip and I want to create a new project for the pinout equivalent in the STM32H7 series. In CubeMX I can generate a pinout listing from my F7 project as a ...

EEPROM endurance, calculation of EEPROM writing cycles

Posted on August 08, 2017 at 11:14Hi all,How is calculated the number of times that a certain byte of the internal STM32(L0) EEPROM is written in the following situation?1 - The firmware writes a byte in EEPROM address 0x0808 0000. The code *(uint8_...

0690X00000607nFQAQ.png
M F by Associate II
  • 2805 Views
  • 2 replies
  • 0 kudos

Interrupt triggered only once

Posted on August 07, 2017 at 22:06  The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32L1 Current consumption in Stop Mode

Posted on August 08, 2017 at 13:35I used CubeMX code generator,Internal Clock 4.194MHz MSI / ADC / LCD / RTC / TIM2 / TIM3 / USART1Before Stop Mode Enter,void Before_Stop_ST(void){ //--- LCD Off LCD_All_Display(0,1); HAL_LCD_MspDeInit(&hlcd); HAL_L...

Why is Assembly language (and/or GNU C) listed multiple times in the ''Include Directories'' section of Eclipse?

Posted on August 08, 2017 at 16:24In project properties - C/C++ General - Paths and Symbols - Includes tabLooking through a few example programs, I'm seeing 3 Assembly language settings and 2 GNU C language settings.  I'm used to seeing one of each ...

0690X00000607hpQAA.png
douglas2 by Associate II
  • 694 Views
  • 0 replies
  • 0 kudos