cancel
Showing results for 
Search instead for 
Did you mean: 

Are there technical limitations on some pins of the Nucleo F767ZI

David Fisher
Associate II
Posted on March 31, 2017 at 07:05

I am trying to get some high speed PWM DMA code working on TIM4 CH3 and TIM4 CH4. I can get the

TIM4 CH3

 signal on D10 but the 

TIM4 CH4 on D9 doesn't output anything. Is there some hardware limitation ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 31, 2017 at 08:38

PD15 TIM4_CH4 seem viable, see if you can drive it up/down as a GPIO, proper AF settings, etc.

It is exported to two pins on the board CN12.48 and CN7.18 (D9)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..