cancel
Showing results for 
Search instead for 
Did you mean: 

I have a STM32F407VG6 DIY board

itsna_azz
Associate II
Posted on March 30, 2017 at 21:18

The board can't function properly, it can be downloaded using ST-LINK but the output doesn't match with the program I wrote. Is it because the oscillator? I watch the oscillator signal and it is different from the right board. The other DIY board has more problems besides the oscillator signal, the VCC pin voltage is 0 V and the reset pin voltage is 0 V. Can anyone help troubleshooting these problems? Thank you.

https://community.st.com/tags♯/?tags=stm32%20stm32f4

https://community.st.com/tags♯/?tags=stm32f4%20oscillator

#stm32-stm32f4 #stm32f4-oscillator
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on March 30, 2017 at 21:40

Start with a schematic of what you've actually created.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nesrine M_O
Lead II
Posted on March 31, 2017 at 11:37

Hi

Az_Zahra.Itsna

,

-Nesrine-