STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Suggestions for MCU Choice

Hi :waving_hand:,  I am designing a midi controller. I want test out using an STM30 MCU, I was wondering if anyone could suggest dev board/ processor? I don't want or need wireless communication (wifi and Bluetooth)I want to run a lot of linier poten...

2fourK by Associate
  • 1473 Views
  • 3 replies
  • 0 kudos

STM32L431CBT6 blocks in HAL_Delay()

Greetings! I am using STM32 for a very first time. I made my custom PCB with 10MHz oscillator. In the Clock Configuration window I have sellected the PLL and the HCLK is set to 80MHz (max for the uC). The outputs are all 80MHz. So I made a simple bli...

stoyanoff by Associate II
  • 2346 Views
  • 7 replies
  • 1 kudos

Resolved! SPI chip select pin

Hello,I need to connect more than 2 MCUs with SPI connection(1 Master, 2Slaves). Here is my Hardware connections :MISO1->MOSI2 && MOSI3MOSI1->MISO2 && MISO3SCK1->SCK2 && SCK3NSS1->NSS2 && NSS3But I don't know how I can select each slave with master (...

parisa by Senior
  • 4788 Views
  • 6 replies
  • 0 kudos

External Loader for STM32H533RE with W25Q32

Hi,I try build loaders for STM32H533RE using its nucleo board but it fails to read any thing using the cube programmer. i tried with nucleo H753 and it worked. i see that u already did loader for the H5 so would u please explain how or maybe update y...

msalem88 by Associate II
  • 2145 Views
  • 6 replies
  • 0 kudos

Resolved! STM32 HyperRAM Memory access issue

Hi,I am starting a new post for visibility, hopefully someone can point me towards the right direction.The setup:MCU: STM32H725HyperRAM: W957A8MFYA5I, /CK is groundedOCTOSPI1 is used, its reference clock is 200MHz, so with the Clock Prescaler I am us...

kacsaaa_0-1740502754143.png
kacsaaa by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

ADC doesn't work

Hi all, I have created a new project for the STM32U575RIT6 microcontroller using the attached .ioc file. On top of the auto-generated code, I have made the following modifications:In main.c:    while (1) { uint32_t bits = 0; uint16_t adc_value =...

proyo by Associate II
  • 1406 Views
  • 3 replies
  • 1 kudos