STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Own custom build STLDR file creation issue

hi,I am trying to build my own STLDR file with STM32H723ZGT6 + w25q128.I could able to build the stldr file STLDR creation with Separate Project 1 but it's not working with external loader  project 2 it's giving down load error while program download...

MMARI.1 by Senior II
  • 2478 Views
  • 5 replies
  • 0 kudos

Resolved! Spi clocks are 4, 5, 6 instead of 8 bits

Hi allI am using the stm32h743 device when using spi 6 to transmit data the clocksare 4, 5, 6 randomly instead of 8 bitswhen configuring spi2 the processor function perfectly.on this device I have already used connection: SPI1, SPI5, ethernet, uart4....

dorong by Associate II
  • 4870 Views
  • 17 replies
  • 3 kudos

Failed to execute MI command after update to IDE

Hi All,I know the dreaded 'Failed to load MI command' error has been much discussed on the forum but I can't find any posts which match this set of circumstances, so hoping somebody can help.My project was working perfectly on STM32G0 but I need to p...

pretoriandave_0-1740427561434.png pretoriandave_1-1740427607194.png

STM32G0 Concurrency Question

I have some data that is accessed from a normal context and also from an IRQ. I am disabling the interrupt to prevent interrupted access. So no concerns there. However, what about forcing both the normal context and the interrupt context to have the ...

Carl_G by Senior III
  • 3054 Views
  • 6 replies
  • 2 kudos

Reading from Flash memory crashes the uC

HiWe are facing problems when reading a data that is written to the flash using the following function?Every time we write in reading the data the micro-controller crashes. Even if I want to see the content of the flash in that particular address usi...

Pejwaak by Associate III
  • 1409 Views
  • 3 replies
  • 0 kudos