STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI gets out of sync

Posted on December 07, 2017 at 16:56Hello,I have a problem with the STM32H743.I have a pluggable SPI connection and the STM32H743 works as a Slave in receive mode.When I pull and plug the connection the NSS, CLK and Data connections toggles and I ge...

twagner by Associate II
  • 2732 Views
  • 3 replies
  • 0 kudos

Question about Level1 Cache STM32F7

Posted on November 08, 2017 at 10:11Hello,I have read several documents about the Cache, but the last sentence in AN4839 (Level 1 cache on SRM32F7 Series) confuses me.' However, If the external device is an ASIC and/or a FIFO, the user must disable ...

DMA returns wrong SPI data

Posted on December 08, 2017 at 10:48Hello everyone.I have a strange problem where my SPI data seems to 'shift' and my DMA goes out of control (I do not have a clue why it is acting as it does). I am developing a program using the STM32L433CC togethe...

Why the device serial number in BlueNRG1 is incorrect

Posted on December 08, 2017 at 08:44I found there is an uniq device serial number in BlueNRG1 datasheet, and it's address in 0x100007F4, but when I try to read it, they are all 0xFF, and the memory content in keil memory dialog is all 0xFF. My board...

cgh21 by Associate II
  • 674 Views
  • 0 replies
  • 0 kudos

Start DFU bootloader.

Posted on December 08, 2017 at 08:32Hello,I'm trying to start the DFU bootloader of an STM32F4 Controller.I have my own bootloader implementation and I try to jump to the DFU bootloader from my bootloader.My Problem is:My Firmware is connected to CA...

Resolved! HAL_UART_RxCpltCallback() is triggered only once

Posted on December 07, 2017 at 10:21 Hello all, I am using STM32F030R8T6 and also using HAL libraries for programming. I am using two UARTs one as a debug UART1 to send various messages to PC and UART2 for communication with Bluetooth module (...

Mrunal A by Associate III
  • 2343 Views
  • 1 replies
  • 0 kudos

Are these appropriate LoRaWAN learning tools

Posted on December 07, 2017 at 03:29I own a NUCLEO-L053R8.Is it appropriate to get a I-NUCLEO-LRWAN1, plug it into the NUCLEO  and use the I-CUBE-LRWAN (STM32CubeExpansion_LRWAN_V1.1.2) to start learning LoRaWAN?Is the NUCLEO-L053R8 with the I-NUCLE...