cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F723 ST-Link FLASH memory-size and erase error

Erwin Reuss
Associate II
Posted on August 15, 2017 at 23:28

1. ST-Link reports the wrong size for the Flash memory. ST-LINK-Utility reports 'Unknown' and the ST-Link CLI reports 4095 kBytes.

2. ST-Link CLI can't erase memory sector 1 at 0x08004000. When using the commandline-switch -SE 0 1 st-link cli reports the following Error:

Memory Sector @0x8000000 erased

Memory Sector @0x8004000 is not erased. Verify the memory protection.

Verifying the Option-Bytes the memory is not protected!!!

Only a full chip erase can resolve this problem.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwin Reuss
Associate II
Posted on August 22, 2017 at 22:59

A new version of ST-Link software is online. The STM32F723-bug is fixed. Thank you.

View solution in original post

4 REPLIES 4
Amel NASRI
ST Employee
Posted on August 16, 2017 at 10:25

Hi

Reuss.Erwin

‌,

Are you using the last version of STLink Utility?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Erwin Reuss
Associate II
Posted on August 16, 2017 at 18:42

Yes of course. I am always using the latest version from the ST homepage. ST-Link Utility v4.0.0.0, STLinkUSBDriver.dll v4.4.0.0 and ST-LINK_CLI.exe v3.0.0.0.

All works perfect, wenn i do a full erase before flashing. But this always takes a long time.

Erwin Reuss
Associate II
Posted on August 22, 2017 at 22:59

A new version of ST-Link software is online. The STM32F723-bug is fixed. Thank you.

Posted on August 23, 2017 at 02:53

V4.1.0  

http://www.st.com/en/embedded-software/stsw-link004.html

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..