STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RS485 Communication is not working properly

Posted on December 08, 2017 at 09:24Hello,I got connected measuring device to my STM32F4 - Discovery board (with Open407V-D board). They are communication via RS 485 bus. Measuring device should provide result of measurement after request., but afte...

STM32CubeMX and syscalls.c

Posted on January 14, 2017 at 18:34Hello,Why doesn't STM32CubeMX not provide a copy of syscalls.c in the application directory tree as part of the code generation step?  Presumably, all users of STM32 are developing bare-metal systems and so there m...

pgregson1 by Associate III
  • 1876 Views
  • 3 replies
  • 0 kudos

SAI1 in stm32f722RET6 ?

Posted on December 08, 2017 at 16:47Hi! I'm new to stm32.  I'm trying to  use stm32f722RET6 with WM8510 audiocodec. In CubeMX only SPDIF TX can be selected for SAI1, (I2S/PCM is inactive) . Is it possible to use SAI2 as master receive (I2S protocol)...

STM32CubeMX unable to transmit over UART6/RS232

Posted on December 08, 2017 at 02:01HI,I have a STM32F07G-Disc1 board attached to a Embest BB board which provides an RS232 Interface. I started the STM32CubeMX, and activated the USART6 in Asynchronous mode and Generated the Default code. The follo...

CubeMX after regenerating the project the user code dissipated

Posted on December 06, 2017 at 13:59I add some code to the files generated by CubeMX. When I regenerate the project, my added code will be deleted.In the main.c is /* USER CODE BEGIN */ and /* USER CODE END*/ but in other files, there is no area whe...

An Ha by Associate II
  • 5220 Views
  • 7 replies
  • 0 kudos

STM32Nucleo pack for IoT node with Wi-Fi: P-NUCLEO-CLD1

Posted on December 07, 2017 at 14:58I like to start a new project based on the STM32Nucleo pack for IoT node with Wi-Fi(STM32 Nucleo-64 development board with STM32F401RE MCU).I need to show some decimal values through a LCD keypad display. Here is ...

NRST pin on STSPIN32F0A

Posted on December 07, 2017 at 10:55NRST � I/O Reset - Device reset input/internal reset output(active low). How can I connect this to a HC-05 bluetooth module?#stspin32f0a #bluetooth #nrst-pin #hc-05

STM32F030 I2C Memory Interface emulation

Posted on December 07, 2017 at 11:33I would like to make my MCU appear as a 256-byte I2C RAM on the I2C bus - then I can have the controlling device simply write to the 'RAM' in  order to communicate.This requires variable length access ( e.g. 'writ...