STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32h750vbt6 adc 16bit 14bit issue

Hello,while using this mcu 16bit adc a strange thing happens.the adc signal is test under a sinusoid signal(0.5Hz from a signal generator), and as shown in the figure at certain level adc keeps unchanged, after leaving this level then the signal incr...

mize_0-1723793714498.png mize_1-1723793728792.png mize_2-1723794431864.png mize_3-1723794529822.png
mize by Associate III
  • 7462 Views
  • 13 replies
  • 2 kudos

STM32H743 with USB C connector

Hello there!I've designed a board based on the STM32H743Zit Nucleo board, but unfortunately, I'm facing difficulties with the USB functionality. I'm unsure if it's a matter of configuration or firmware. When I tested USB settings and functionality us...

kmh011 by Associate II
  • 1230 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743VIT6 USB not working

Hello there! Esteemed ST team member,I hope this message finds you well. I'm reaching out to address an issue I've encountered.I've designed a board based on the STM32H743 Nucleo board, but unfortunately, I'm facing difficulties with the USB function...

Schematic_1.png Schematic_2.png
BrunoS by Associate
  • 3520 Views
  • 2 replies
  • 1 kudos

Why is the DBP bit not set to '1'

Hello, I designed a similar board using STM32H743ZIT6 and STM32H743VIT6. (Rev. V)The board works fine normally.It has been in production for 3 years already. Boards that have already been produced and shipped sometimes become unusable. (since a few m...

STM32H7S3L8 SPI Tx DMA burst

Hi,I am trying to use SPI6 transmission with GPDMA on STM32H7S3L8.While Tx transfer works with simple IT handling, it doesn't work with DMA. No way...To take things simple, I am trying a simple burst transfer (I will leave linked list for later), so ...

simo zz by Senior II
  • 1101 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H755 HTRIM PIN high after POR

I'm working with a boost converter and have noticed that when resetting the device a PWM pin remains high/floating for a 100-200msI use the HRTIM with complementary inputs and deadtime insertion.If my lowside pin remains floating/high for an extended...

kip18 by Associate III
  • 767 Views
  • 1 replies
  • 0 kudos